Entitlements
Two entitlement types are available for
FactoryTalk®
Remote Access™
: domain and Runtime entitlements.
NOTE:
See How to activate a entitlement to learn how to activate an entitlement.
See Entitlements in the
FactoryTalk®
Hub™
online manual for further information on entitlement
purchasing and allocation.Entitlement types and upgrades
- Allows HMIs or IPCs to connect toFactoryTalk® Remote Access™Runtime entitlements:FactoryTalk® Remote Access™and determine the operations that are granted by that connection. Devices are provided by default with a Runtime entitlement that may consist of aProorBasicentitlement.NOTE: To learn more about what license is assigned to each device by default, see the device sections listed under System components.You can upgrade any Basic entitlements by purchasing a Pro license on the Commerce Portal for your organization.The Pro entitlement upgrade allows yout to obtain extra features. This means that the Basic entitlement remains assigned to the device and you cannot rehost the Basic entitlement to other devices.NOTE:
- If you want to detach a Basic entitlement, you must first detach any Pro entitlement upgrades, if present.
- If you remove a device from a domain, any entitlements assigned to it become available for rehosting.
See the table below for further information about the Basic and Pro entitlements:EntitlementDescriptionFactoryTalk® Remote Access™Runtime BasicBasic entitlements allow file transfers, task management, and minimal VPN capabilities.NOTE: OptixPanel™ Compact graphic terminals display anUpgradebutton next to the Basic entitlement type, in the right pane of theDomain view, in the Entitlements section. This button allows you to upgrade the Basic entitlement to the Pro entitlement by purchasing just the services that are not already included in the Basic entitlement.FactoryTalk® Remote Access™Runtime ProPro entitlements allow VPN access to all devices on the device network, file transfers and task management. - This domain entitlement may be purchased in volumes of 1/2/5/10/25/50 concurrent device connections.FactoryTalk® Remote Access™1/2/5/10/25/50 Concurrent Connections entitlements:
- This entitlements bundle includes a domain entitlement for concurrent connections and four Runtime entitlements. It consists of a temporary entitlements bundle including:FactoryTalk® Remote Access™Trial Bundle:
- FactoryTalk® Remote Access™2 Concurrent Connections entitlement*
- TwoFactoryTalk® Remote Access™Runtime Basic entitlements
- TwoFactoryTalk® Remote Access™Runtime Pro entitlements
*Once the Trial Bundle is activated by your Sales Representative, you will find the newly assigned domain inFactoryTalk® Remote Access™Manager.NOTE: See Trial Entitlements in theFactoryTalk® Hub™manual for further information on this subject.
Entitlements expiration
When an entitlement expires, the domain connected to it expires too.
- are perpetual, including Runtime entitlement upgrades.FactoryTalk® Remote Access™Runtime entitlements
- expire after 365 days and a 7-days grace period following the expiration date activates to allow for entitlement renewal through theFactoryTalk® Remote Access™1/2/5/10/25/50 Concurrent Connection entitlementsFactoryTalk® Hub™. If the entitlement is not renewed within the grace period, the user can still access the domain, without being able to carry out any action within it.Select the entry to allow each admin and owner user to receive an email every day during the grace period, informing them about any days left to the entitlement expiration.NOTE: 60, 30, and 10 days before theexpires, an email is sent to all of the admin and owner users to inform them about the expiration deadline.FactoryTalk® Remote Access™1/2/5/10/25/50 Concurrent Connection entitlement
- FactortyTalk Remote Access Runtime Trial Bundle:The Runtime entitlements included in the Trial Bundle expire when theFactoryTalk® Remote Access™2 Concurrent Connections entitlement expires. After expiration, no grace period starts.NOTE: For details about your Trial Bundle subscription duration and expiration date, contact your Sales Representative.NOTE: Notification messages will appear each time you log on to the service informing you of the number of days remaining in the Trial Bundle entitlement. After the trial period is over, you will not be able to use the service until you obtain a subscription.
NOTE:
You can register a device to a domain while the same device is registered to another domain.
See your entitlements in FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
- AccessFactoryTalk® Remote Access™Manager.
- In thePermissions/Informationpane, openEntitlements. This section shows the entitlements for both domains and device Runtimes in your organization.NOTE: In this area, you can see how many entitlements have already been assigned and how many are still available to you.
See your entitlements in FactoryTalk®
Hub™
FactoryTalk®
Hub™
Provide Feedback