Delete a connection to a program parameter
Delete a connection to a program parameter to stop passing the data from the parameter into and out of the program for a controller tag, device tag, or other program tag.
- On the explorer bar, select
Systemand then select the program. - In theSystemtitle bar, Select
View tags and parameters. The Tag Editor opens.TIP: To open the Tag Editor, you can also right-click the program and selectTags and parameters. - On the Tag Editor, select the parameter.
- InProperties, selectConnections.TIP: IfPropertiesdoes not open, in the pane bar, select
Properties. - Next to the connection to delete, select
Delete. - (optional) To undo the deletion, in the toast, selectUndo.
Provide Feedback