Find a function within a DLL file

An external routine DLL must call a function. Use the
Functions Available
dialog to choose a function from a list.
To find a function within a DLL file
  1. From the Controller Organizer right-click the active routine and then choose
    Properties
    .
  2. Click the
    Configuration
    tab, and then click the
    Browse
    dots button.
  3. From the list of available functions, choose the function that the external routine calls.
  4. Select
    OK
    to close the
    Functions Available
    dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal