Delete a program

A program contains routines, including a main routine, and tags and is scheduled in a task.
Delete programs either from the
Controller Organizer
or the
Logical Organizer
. Deleting a parent program also deletes its descendant programs.
The
Delete
command is disabled if:
  • Security does not allow deleting the program.
  • The immediate parent of the program is a program or a folder that security does not allow deleting
If the project is offline, delete a program from the organizer without having to unschedule the program and delete its routines and tags.
To delete a program:
  1. If the project is online, unschedule the program to delete from the task in which it is scheduled.
  2. Select the program in the Controller Organizer or Logical Organizer.
  3. From the
    Edit
    menu, choose
    Delete
    .
  4. Click
    Yes
    to confirm the deletion.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal