PTST parameters

Use the
General
tab of the
PTST Properties
dialog box to monitor the parameters for the selected Process Tank Strapping Table (PTST) instruction or function block.
To monitor parameters for PTST instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. View the read-only parameters:
    • Gross volume
      . The gross observed volume.
    • Free water volume
      . The free water volume (barrels, gallons, liters).
    • Raw volume
      . The raw total observed volume from calibration table (barrels, gallons, liters).
    • Calculated tank temperature
      . The calculated tank shell temperature (degrees Fahrenheit or Celsius).
    • Correction for tank temperature
      . The correction for temperature of tank shell (multiplier).
    • Floating roof adjustment volume
      . The floating roof adjustment volume (barrels, gallons, liters).
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal