Message Configuration Dialog Box - Configuration Tab Overview

After you enter the MSG instruction and specify the MESSAGE structure, use the
Message Configuration
dialog box to specify the details of the message.
The details you configure depend on the message type you select.
Message Configuration Tab
If the target device is:
Select one of these message types:
Logix 5000 controller
CIP Data Table Read
CIP Data Table Write
I/O module that you configure by using Logix Designer application
Module Reconfigure
CIP Generic
PLC-5 controller
PLC-5 Typed Read
PLC-5 Typed Write
PLC-5 Word Range Read
PLC-5 Word Range Write
SLC controller MicroLogix™ controller
SLC Typed Rated
SLC Type Write
Block transfer module
Block Transfer Read
Block Transfer Write
PLC-3 processor
PLC-3 typed read
PLC-3 typed write
PLC-3 wood range read
PLC-3 wood range write
SERCOS module
SERCOS IDN Read/Write
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal