Safety State

Displays the current state of the CIP Safety drive. These states include:
  • Unknown (No Motion Connection)
  • Self-Testing
  • Configured (No Safety Connection)
  • Self-Testing Failed
  • Running
  • Not Running
  • Recoverable Fault
  • Unrecoverable Fault
  • Configuring
  • Not Configured
  • Unknown
  • Not Configured (Torque Permitted)
  • Not Running (Torque Permitted)
The Safety State is available only when the drive is a CIP safety drive.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal