Failed to modify component properties

One of these conditions prevents the modification of the component properties:
  • Access denied. Verify with your Security Administrator that you have sufficient privileges to modify the component.
  • Entered an already existing or invalid name. Enter a unique and valid name for the component.
  • Attempted to change the component's class (for example, standard versus Safety) while the component is already scheduled in a task. Remove the schedule from the component and then change the class.
  • The controller is locked by another user in another instance of the
    Logix Designer
    application.
  • The fault routine of an equipment phase cannot have PSC, PFL, PXRQ, PPD, or PRNP instruction calls.
  • The prestate routine of an equipment phase cannot have PSC, PXRQ, PPD, or PRNP instruction calls.
  • Attempted to change the component's class to Safety but the component contains a tag with OPC UA access set to RW. Remove the OPC UA access and then change the class.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal