Export Project Documentation dialog box overview

Use the Export Project Documentation dialog box to specify the name and location of the exported localization file.
These are the parameters for the Export Project Documentation dialog box.
Table Heading
Table Heading
Localization File Name
Displays an automatically generated name based on the choices you made on the previous dialog boxes of the export wizard. You may change this name.
The localization file has a .txt extension. If you do not add the .txt extension to a file name, it is added for you.
Location
The file path to the location where the localization file is to be created.
The default is the default project file location or the last location used on the workstation is remembered.
Browse
Opens the Browse for Folder to locate where you wish to export the file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal