Create Custom Language dialog box overview

Use the
Create Custom Language
dialog box to configure a new custom language.
  • Name
    . Enter a unique name for the custom language follow the RFC1766 Naming Conventions.
  • Root Language
    . Select a root language to associate with the custom language. Root languages cannot be custom languages. If a root language is specified, the custom language appears along with the root language in lists such as the Localize To list in the export wizard. By default the Root Language is
    None
    .
  • Full Name. The custom language prefixed with the RFC1766 name of the specified root language. When a root language is not specified, the name is prefixed with x-.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal