Configuring Message Instructions

To configure message instructions:
  1. From the
    Message Type
    menu, select the type of message you want to send. Depending on the type of message you choose, various parameters appear on the
    Configuration
    tab of the
    Message Configuration
    dialog box. Follow the steps below, depending on the type of message you have chosen. See
    Message Configuration Dialog Box - Configuration Tab Overview
    for descriptions of all the parameters and fields available on the
    Configuration
    tab.
  2. From the
    Service Type
    menu, select the desired service, if applicable. Depending on the service type selected, the remaining fields on the dialog box are enabled/populated, or disabled.
To complete the remaining fields/parameters:
  • Locate the desired Message Type below for instructions on completing the remaining fields/parameters on the dialog box.
Generic CIP
TIP:
Selecting the CIP Generic message type enables the Large Connection option on the
Communications
tab. The Large Connection option provides the ability to configure CIP Generic type messages to use either a standard 502 byte connection size or a large 4002 byte connection size.
  1. In
    Service Code
    , enter the hex value for the service that is to be performed on the specified object.
  2. In
    Class
    , enter the hex value for the type or class of object to which the service is to be sent.
  3. In
    Instance
    , enter the instance of the object to which the service is to be sent.
  4. In
    Attribute
    , enter the hex value of the attribute of the object to which the service is to be sent.
  5. From the
    Source
    menu, choose a local source tag that contains additional service parameters and/or data that is to be sent with the service.
  6. In
    Number of Elements
    , enter or choose the number of bytes of data from the source tag that will be included with the service request.
  7. From the
    Destination
    menu, choose a local destination tag that will contain data received from the service. The data will be requested information or additional information from the extended error.
    TIP:
    Depending on the service type selected, source or destination, tags may not be required. It is also important that you create the destination tag with the appropriate size so that it can contain all the data to be returned.
  8. Select
    New Tag
    to create a new tag.
CIP Data Table Read
  1. In
    Source Element
    , enter the source data table element to read. This is the remote data table element.
    TIP:
    To point to Program Scope tags on a remote device, use the syntax:
    Program:<program_name>.<tag_name>
    For example, to read a tag named MyTag that is in the program scope in a program named Pump_Control on a remote controller, the correct syntax for
    Source Element
    is:
    Program:Pump_Control.MyTag
  2. In
    Number Of Elements
    , enter or choose the number of elements or integers of data to read from the source element.
  3. From the
    Destination Element
    menu, choose the local tag in which to place the read information.
  4. Select
    New Tag
    to create a new tag.
CIP Data Table Write
  1. From the
    Source Element
    menu, choose the local tag that contains data with which to write.
    TIP:
    To point to Program Scope tags on a remote device, use the syntax:
    Program:<program_name>.<tag_name>
    For example, to write a tag named MyTag that is in the program scope in a program named Pump_Control on a remote controller, the correct syntax for
    Destination Element
    is:
    Program:Pump_Control.MyTag
  2. In
    Number Of Elements
    , enter or choose the number of elements or integers of data to write from the source tag.
  3. In
    Destination Element
    , enter the destination data table element into which the data will be written.
  4. Select
    New Tag
    to create a new tag.
Block Transfer Read
  1. In
    Number of Elements
    , enter or choose the number of 16-bit integers of data to transfer.
  2. From the
    Destination Element
    menu, choose the local tag to place the read transfer into.
  3. Select
    New Tag
    to create a new tag.
Block Transfer Write
  1. From the
    Source Element
    menu, choose the local tag that contains data to transfer.
  2. In
    Number of Elements
    , enter or choose the number of 16-bit integers of data to write from the Source Tag.
  3. Select
    New Tag
    to create a new tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal