Build command

Select this command to add project data to the cache to speed up project downloads. The build process verifies and caches routines, and the cached files are included when the project is downloaded to the controller, reducing download time. The
Build
command is available only when the controller is offline.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal