Compatible Safety Controllers
A safety controller is required for use in Network mode control (‘Safety’, ‘Standard and Safety’, or ‘Motion and Safety’ used for Connection type). The following safety controllers can be used:
Controller | Firmware Revision |
---|---|
GuardLogix® 5580 controller | 31 (or later) |
Compact GuardLogix® 5380 controller | 31 (or later) |
IMPORTANT:
The Integrated Safety Functions option module is not supported by
GuardLogix®
5570 and Compact GuardLogix®
5370 (or earlier) safety controllers.Provide Feedback