Connection View
Use Connection to define controller-to-device behavior:
- Set the RPI rate. For more information, see Requested Packet Interval.
- Select Unicast or Multicast connection to use on the EtherNet/IP network. For more information, see Unicast or Multicast Connection.
- View the reason of Connection Fault.TIP: If there is a connection fault, Connection Fault area displays the error code with description that helps you to troubleshoot the module. For more information, see Troubleshoot Your Module.
- Inhibit the module. For more information, see Module Inhibiting.
- Configure fault response for connection failure while the controller is in Run Mode.
- Enable or disable the Automatic Diagnostics.ATTENTION: If you do not enable Automatic Diagnostics, the device does not publish diagnostics to FatoryTalk Alarms and Events.
Connection View Example

Recommended Minimum RPI Values for Notch Filters
In the following table, each Notch Filter setting has two recommended minimum module
RPI values that allow the required time to collect samples from each channel. One
setting provides faster sample speed and the other provides slightly better
resolution at slower sample speeds.
Notch Filter (Hz) | Recommended Minimum Module RPI
Value | |||
---|---|---|---|---|
Application That is Configured With Only
One Channel Enabled | Application With All Channels Enabled
and Using the Same Notch Filter Setting on All Channels | |||
Faster Sampling Speed (ms) | Better Noise Rejection (ms) | Faster Sampling Speed (ms) | Better Noise Rejection (ms) | |
10 | 106 | 316 | 422 | NA |
20 | 53.1 | 158.1 | 212 | 632 |
50 | 22 | 64 | 86 | 254 |
60 (default) | 18.3 | 53.2 | 72 | 212 |
100 | 11.2 | 32.1 | 44 | 127 |
200 | 5.9 | 16.4 | 22.2 | 65 |
400 | 3.5 | 8.6 | 12 | 33 |
500 | 2.8 | 6.9 | 9.3 | 26.5 |
1000 | 1.7 | 3.8 | 5.2 | 13.5 |
5000 | 1.0 | 1.3 | 2.2 | 3.3 |
10000 | 0.7 | 0.9 | 1.7 | 2.1 |
15625 | 0.8 | 0.8 | 1.7 | 1.7 |
31250 | 0.4 | 0.6 | 1.2 | 1.5 |
Minimum RPI Calculation When Using Different Notch Filter Selections
When input channels on the same module use different Notch Filter selections, you
must consider the sample time for each channel. This helps you to find the
recommended RPI that provides enough time for sampling all channels.
The eight input channels on the module are grouped into two groups. Channels 00…03
are grouped, and channels 04…07 are grouped. When you determine the recommended
minimum module RPI value, remember:
- The recommended minimum module RPI value when channels use different Notch Filter selections is determined by group.The recommended minimum RPI rates for all enabled channels added together. If any channel in the other group is enabled, the recommended minimum RPI rate for each enabled channel is increased by 0.2 ms.
- If the groups have different recommended minimum RPI values, use the higher RPI value when you configure the module.
Channel Group | Channel | Notch Filter (Hz) | Recommended Minimum Module RPI for Each Channel
(ms) (1) | Recommended Minimum Module RPI (ms) | Recommended Minimum Module RPI to Use in Module Configuration
(ms) |
---|---|---|---|---|---|
Grouped together | Ch00 | 50 | 22.2 | 24.7 | 74.0 |
Ch01 | 1000 | 1.9 | |||
Ch02 - Disabled | N/A | N/A | |||
Ch03 | 31250 | 0.6 | |||
Grouped together | Ch04 | 60 | 18.5 | 74.0 | |
Ch05 | 60 | 18.5 | |||
Ch06 | 60 | 18.5 | |||
Ch07 | 60 | 18.5 | |||
(1) The values in this column represent the corresponding
recommended minimum RPI value listed in Table 1 with an
additional 0.2 ms added to it because at least one channel
is enabled in the other group. |
Channel Group | Channel | Notch Filter (Hz) | Recommended Minimum Module RPI for Each Channel
(ms) (1) | Recommended Minimum Module RPI (ms) | Recommended Minimum Module RPI to Use in Module Configuration
(ms) |
---|---|---|---|---|---|
Grouped together | Ch00 | 50 | 64.2 | 69.0 | 213.6 |
Ch01 | 1000 | 4 | |||
Ch02 - Disabled | N/A | N/A | |||
Ch03 | 31250 | 0.8 | |||
Grouped together | Ch04 | 60 | 53.4 | 213.6 | |
Ch05 | 60 | 53.4 | |||
Ch06 | 60 | 53.4 | |||
Ch07 | 60 | 53.4 | |||
(1) The values in this column represent the corresponding
recommended minimum RPI value listed in Table 1 with an
additional 0.2 ms added to it because at least one channel
is enabled in the other group. |
Provide Feedback