Calibration Impacts Data Quality
When a channel on an analog input module is being calibrated, the Notch Filter setting
for that channel changes to 10 Hz. The I.Chxx.Uncertain tag is set to 1 for that channel
until calibration is completed.
Grouped inputs share an Analog-to-Digital converter. As a result when any input channel
is in the calibration process, the
I.Chxx.Uncertain
tag is set to 1 for other
input channels in that group. This is because the data sampling rate slows for all input
channels in the group.Provide Feedback