Assign main and fault routines

Use the
Configuration
tab of the
Program Properties
dialog box to assign main and fault routines for your program.
To assign main and fault routines:
  1. From either the Controller Organizer or Logical Organizer, right-click the program to change and choose
    Properties
    .
  2. Choose the routine to designate as the main routine from the
    Main
    menu in the
    Assigned Routines
    frame.
  3. Choose the routine to designate as the fault routine from the
    Fault
    menu in the
    Assigned Routines
    frame.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal