Confirm controller type change

After selecting
Change Type
in the
Change Controller
dialog box, confirm to change the controller type.
Carefully read the consequences of the change that are listed on this screen. Then select
Yes
to continue with the change or
No
to keep using the existing controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal