Change Controller Fault Handler online

This message appears while you are online in Remote Program mode, and you drag a program to or from the Controller Fault Handler program folder (from or to the Unscheduled Programs folder).
  • If you are dragging to the Controller Fault Handler folder from the Unscheduled Programs folder and you click OK, the current Controller Fault Handler program (if there is one assigned) will be moved to the Unscheduled Programs folder, and that program that you were dragging will become the new Controller Fault Handler program.
  • If you are dragging from the Controller Fault Handler folder to the Unscheduled Programs folder and you click OK, the current Controller Fault Handler program (i.e., the program you are dragging) will be moved to the Unscheduled Programs folder and there will be no assigned Controller Fault Handler program.
  • If you press Cancel, programs will remain where they were prior to the beginning of the drag-and-drop operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal