Connection Settings
The advanced settings of connection ports and proxy server allow the Tool to connect to the
network infrastrutture and establish a VPN
connection with the remote device.
FactoryTalk®
Remote Access™
To configure network port and proxy settings for VPN connections:
- Access theand select .FactoryTalk® Remote Access™ManagerNOTE: When clicking onConnection settings, a dialog window will show up asking for permission to open theConnection settingsTool. Prior to confirming, flag theAlways allowcheckbox to prevent this message from prompting again during this session. If you use a different computer or a different browser, this message will prompt again.
- Under select the network port to use for VPN connections.
- Auto:The Tool automatically selects the appropriate port based on the connection request.
- 80:The Tool will only attempt to establish a remote access using the HTTP protocol over port 80. If the connection over port 80 is rejected, the session is not established.
- 443:The Tool will only attempt to establish a remote access using the HTTP protocol over port 443. If the connection over port 443 is rejected, the session is not established.
- 5935:The Tool will only attempt to establish a remote access using the HTTP protocol over port 5935. If the connection over port 5935 is rejected, the session is not established.
- If a proxy service is used for internet connections, select the type of proxy server underProxy:
- None:A proxy server is not used for the internet connection.
- HTTP:HTTP Proxy Server. Forwards HTTP requests.
- SOCKS5:SOCKS5 Proxy Server. Forwards TCP and UDP packets.
NOTE: See Proxy for further information on this subject. - After making your selections, clickApplyto save the proxy settings to the domain.
Once the connection to the remote device is established, if the device is disconnected, it will enter a timeout mode while it automatically attempts to reconnect. In this situation, a warning icon displays while attempting to reconnect.
Provide Feedback