Configure features supported in the container
Runtime is designed as a multi-container application, which means you can use Docker Compose to run it.
Set the environment variables in the .env file according to the environment variables that best suit your needs before executing the Docker Compose command. The .env file should look like this:
SETUPHOSTIMAGE=factorytalkremoteaccess/setuphost RUNTIMEIMAGE=factorytalkremoteaccess/runtime TAG=<version> SETUPHOSTCONTAINER=factorytalkremoteaccess-setuphost RUNTIMECONTAINER=factorytalkremoteaccess-runtime VERBOSE=false VOLUME= TZ=UTC APPARMOR_PROFILE=factorytalkremoteaccess_runtime WEB_LOGIN_PASSWORD= RDP_DISPLAY= RDP_XAUTHORITY= VPN_ADAPTERS= VPN_P2P=false
Variable | Definition | Note |
|---|---|---|
SETUPHOST_IMAGE | Specifies the image name of the Setuphost service. | ALREADY SET |
RUNTIME_IMAGE | Specifies the image name of the Runtime service. | ALREADY SET |
TAG | Defines the tag for both images. | ALREADY SET |
SETUPHOST_CONTAINER | Indicates the container name associated with the Setuphost service. | ALREADY SET |
RUNTIME_CONTAINER | Indicates the container name associated with the Runtime service. | ALREADY SET |
VERBOSE | Enables detailed output from the Setuphost in operation if set to true . The default value is false . | EDITABLE |
VOLUME | Specifies the path to the volume mounted by the Runtime to store persistent data. For example, /path/to/persistent/folder . | SET MANDATORILY |
TZ | Sets the time zone where the Runtime operates. By default, the time zone is set to UTC . You can change this preset time zone by modifying the UTC value. | EDITABLE |
APPARMOR_PROFILE | Defines the AppArmor profile applied to the Runtime service. To run the container without complying with any security policies, remove this variable or set it to unconfined . | EDITABLE |
WEB_LOGIN_PASSWORD | Protects the Web UI of the Runtime through a password. This variable is not set by
default, but it is recommended to set it for security purposes. This value is
entered into the Setuphost service as a secret. | EDITABLE |
RDP_DISPLAY | Specifies the host display used by the Runtime to run the Remote Desktop feature. See Enable the Remote Desktop Protocol (RDP). | SET ONLY FOR RDP |
RDP_XAUTHORITY | Specifies the path to the .Xauthority file used by the standard user that interacts with the X11 server. See Enable the Remote Desktop Protocol (RDP). | SET ONLY FOR RDP |
VPN_ADAPTERS | Specifies the interfaces with which the Runtime can establish VPN connections. See Enable a VPN connection. | SET ONLY FOR RDP |
VPN_P2P | Enables the Point-to-Point VPN feature in Runtime if set to true . The default value is false . | SET ONLY FOR RDP |
Provide Feedback