Language setup
- During the installation of Tools or Runtime, select your preferred language when prompted by the installer.NOTE: To select a different language than the one chosen during your previous installation, reinstall the Tools. You can choose your preferred language at every Runtime update.
- When you start, select the language by clicking theFactoryTalk® Remote Access™Manager
button at the top-right corner.NOTE: On your first access,will use the language set in your browser, if supported. If the browser language is not supported, the application will open in a default fallback language.FactoryTalk® Remote Access™Manager
Provide Feedback