Request Assistance
You can determine which user accounts in your domain are allowed to receive assistance
requests and for which devices. Once you have granted at least one user account in the domain
to receive assistance requests, the operators of the selected remote devices can use
that intervention is required on the
system.
Request Assistance
from a remote device to inform the FactoryTalk®
Remote Access™
Manager
NOTE:
Device installer
permissions are required to enable or
disable the Request Assistance
entry. See Domain user permissions for further information on this
subject.To enable a remote device to request assistance:
- Sign in to thedomain using an administrator account.FactoryTalk® Remote Access™Manager
- Access the section.
- Select the remote device in the left pane.
- Scroll the right pane until you reach theSubmit assistance requestsentry and flag it.
- To limit the assistance time frame for security reasons, enter a date in theExpiration datefield. After that date, assistance requests for that specific remote device will no longer be permitted.
When
Submit assistance requests
is enabled on a remote device, the user operating it can click on the Request Assistance
button showing up on the Windows Runtime Network connection
section of the remote device to submit an assistance request.If the domain entry
The user must provide contact details when assistance is requested
is enabled, the user operating the remote device will be prompted to populate the Name
, Contact information
and Description
fields to submit an assistance request.
NOTE:
See FactoryTalk Remote Access Manager overview and related entities to view the Assistance required toggle switch in the application.
NOTE:
If both
Require contact details when requesting assistance
and Submit assistance requests
are enabled, the user of the Runtime device can provide a comment while sending their assistance request. The text in the comment shall not include ../
, because this text string might be considered as a path traversal attack.Assistance request notifications
A user registered to the that is required to give assistance
will be notified as follows:
FactoryTalk®
Remote Access™
Manager- They will receive a pop-up notification showing the assistance request.
- They will receive an email to the account related to the concerned domain in theAssistance request notification emailsetting.
NOTE:
You can activate both notification options or one of them, as needed.
NOTE:
In the right pane, the remote devices for which
Request Assistance
has been activated are identified with a small red bell
icon.Cancel or close an assistance request
It is possible to cancel an assistance request from Windows Runtime or close one from the
.
FactoryTalk®
Remote Access™
ManagerAn assistance request can be closed from the by accessing the right pane in and selecting
FactoryTalk®
Remote Access™
ManagerClose
if a resolution has been
provided.If support is no longer needed, a user can cancel the assistance request by accessing the Windows Runtime of the remote device and selecting
Cancel request assitance
from the Network Connection
section.Provide Feedback