Purchase a FactoryTalk Optix Pro entitlement
FactoryTalk Optix Studio Pro is available by subscription only. FactoryTalk Optix Runtime is only available with a perpetual license. Purchase and allocate or assign an entitlement or license to an organization in order to activate FactoryTalk Optix Pro. You must have a purchase order to purchase software.
Devices that are not activated operate in demo mode and stop running
FactoryTalk Optix Applications
after 2 hours. The Emulator
client that runs FactoryTalk Optix Applications
on the development computer does not require a runtime license.- From the Commerce Portal, log in to your MyRockwell account.
- Scroll to FactoryTalk Optix and under FactoryTalk Optix, selectContinue.
- Select your package, scroll to select options to customize your package, and then underSelect Quantity, select the number of entitlements.
- SelectADD TO CART. You can change the number of entitlements in your cart.TIP: If you copied a FactoryTalk Optix Runtime catalog number from the Runtime Sizing tool, you can paste the selected catalog number in the search bar at the top of the Commerce Portal page. Paste the catalog and select
to add the catalog number to your cart. - Review your cart and the pricing with your Distributor and then selectCHECKOUT.
- Confirm your shipping, billing, contract details, and order summary and then selectSUBMIT ORDER.
- On the confirmation page, selectManageLicensesand confirm your new contract.
Once the license status is active, the entitlement appears in FactoryTalk Hub. You can also confirm your order status in the Commerce Portal by selecting
My Subscriptions/Manage Licenses
. Provide Feedback