Runtime entitlements and feature tokens for target devices
Runtime entitlements differ between target devices.
Device type | Pre-assigned entitlement | Upgrade available | Maximum entitlement |
|---|---|---|---|
Edge Compute | XS 5 feature tokens | Yes | L 15 feature tokens |
OptixPanel™ Compact | S 8 feature tokens | Yes | M 11 feature tokens |
OptixPanel™ Standard | M 11 feature tokens | Yes | L 15 feature tokens |
ASEM™ 6300 Industrial PCs | none | No | XL 21 feature tokens |
TIP:
If you need to purchase additional entitlements for an
ASEM™
6300 device, remove the existing entitlement from the device and place it back on the Optix Portal. You can then purchase a new entitlement of a different size. You can reuse the previous entitlement on another device.Provide Feedback