Channel Status Indicators
Indicator State | Description | Recommended Action |
---|---|---|
Off | One of the following conditions exists:
| Complete one of the following:
|
Steady yellow | The input channel is operating normally. | None |
Flashing red | One of the following conditions exists:
| Complete one of the following:
|
Flashing yellow/red | Calibration is in progress. | Successfully complete the calibration process. |
Steady red | An issue has occurred that is internal to the module. The
following are example issues that can cause the status indicator
to be steady red:
| Complete one of the following:
|
Provide Feedback