Add a New Module to a Studio 5000 Logix Designer Application Project

You must complete the following tasks before you configure the module:
  1. Create a Studio 5000 Logix Designer application project.
  2. Add a Logix 5000 controller to the project.
  3. Add a PointMax EtherNet/IP adapter to the project.
    For more information on how to add a PointMax EtherNet/IP adapter to the Studio 5000 Logix Designer application project, see the PointMax EtherNet/IP Adapter User Manual, publication 5034-UM001.
After completing above steps, add your I/O module to the project by following one of the methods:
  • Discover Modules
  • New Module
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal