New program dialog box settings

Use the
New Program
dialog box to create a new program.
Parameter
Description
Name
Enter a name for the new program.
Description
Enter a description of the program.
Parent
To make this program a child of an existing program in the logical model, select the parent program. Otherwise select <none>.
This field is disabled when Controller Fault Handler or Power-Up Handler is selected in the Schedule In field.
Class
Indicates whether the program is a Standard program or a Safety program.
This value applies to Safety applications only.
Use as Folder
Select to create a program folder rather than a program.
When the check box is selected, the
Schedule In
,
Inhibit Program
, and
Synchronize Redundancy Data after Execution
parameters are disabled. If a value is selected for the
Schedule In
parameter it is reset to <none>.
TIP: The
Synchronize Redundancy Data after Execution
option only applies to standard controllers; it does not apply to Safety controllers.
If
Controller Fault Handler
or
Power-Up Handler
is selected in the
Schedule In
field, the
Use as Folder
check box is disabled.
Schedule In
Choose the task in which you want the program to be scheduled.
Inhibit Program
Select to prevent the program and its routines from executing.
Synchronize Redundancy Data after Execution
Choose to synchronize redundancy data after execution (check box is selected) or not to synchronize redundancy data after execution (check box is cleared). The check box is selected by default.
TIP: The
Synchronize Redundancy Data after Execution
option only applies to standard controllers; it does not apply to Safety controllers.
Check box is not shown for non-Redundancy catalog numbers. Check box is always selected for controllers with Redundancy enabled. Check box is disabled when Redundancy is not enabled.
OK
Click to accept the information entered and create the new program.
If online, the program is created in the controller.
Cancel
Click to cancel the creation of this program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal