Tasks, programs, and routines

A project file contains the building blocks of the control system.
Tasks are the basic scheduling mechanism for executing a program. The default configuration contains a continuous task, called Main Task.
The Main Task contains a program called Main Program.
The Main Program contains a routine called Main Routine, which is configured as the main routine.
The system executes the task, programs, and routines defined in the project from beginning to end.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal