Open from Source Control command

Choose this command to open a project file from source control. If a project is already open, the project closes. If the open project was modified, a prompt opens to save the project.
This menu item is only available if the Places Bar in the Open/Import Project dialog box is disabled. When the Places Bar is enabled, use the
Source Control
button in the Open/Import Project dialog box to open project files from source control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal