NegSoftOvertravelFault

Applies to: Servo and Servo Drive axes.
NegSoftOvertravelFault is a Boolean attribute and occurs when the axis has traveled, or attempted to travel, beyond the setting for Maximum Negative Soft Travel Limit, as set in the Limits tab of a Servo axis properties dialog box or in the Limits tab of a Servo Drive axis properties dialog box.
NOtrvlFault or NegSoftOvertravelFault is a recoverable condition.
To clear a NegSoftOvertravelFault:
  1. Restore the axis back within its normal operation limits, either manually or with planners. As soon as the axis is returned back within these travel limits, the Negative Software Overtravel Fault is cleared.
  2. Be sure your program or fault handling routine contains either a:
    • Fault Reset (MAFR) instruction, to clear all motion faults for an axis, or
    • Shutdown Reset (MASR or MGSR) instruction to return to the axis ready operating state.
The occurrence of a NegSoftOvertravelFault sets bit #1 of the respective DriveFault or ServoFault attribute, the PhysicalAxisFault attribute, and bit #0 of the AxisFault attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal