Danger: Scheduling programs online will affect logic execution

You are attempting to schedule a program or programs while the system is online by dragging them from the Logical Organizer to a standard or a Safety task in the Controller Organizer. If any of the dragged programs have descendants (child items) in the
Logical Organizer
, the descendants are included with the parent items. Scheduling programs while online changes the execution of programs and may have unintended consequences.
Select
OK
to schedule the program(s), or select
Cancel
to not schedule the program(s).
You cannot do the following when online:
  • Drag and drop a standard program to a Safety task in the
    Controller Organizer
    .
  • Drag and drop a safety program to a standard task in the
    Controller Organizer
    .
  • Reschedule any currently scheduled programs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal