Change Power-Up Handler while online

This message appears while you are online in Remote Program mode, and you drag a program to or from the Power-Up Handler program folder (from or to the Unscheduled Programs folder).
  • If you are dragging to the Power-Up Handler folder from the Unscheduled Programs folder and you click OK, the current Power-Up Handler program (if there is one assigned) will be moved to the Unscheduled Programs folder, and that program that you were dragging will become the new Power-Up Handler program.
  • If you are dragging from the Power-Up Handler folder to the Unscheduled Programs folder and you click OK, the current Power-Up Handler program (i.e., the program you are dragging) will be moved to the Unscheduled Programs folder and there will be no assigned Power-Up Handler program.
  • If you press Cancel, programs will remain where they were prior to the beginning of the drag-and-drop operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal