Process Variable Speed Drive (PVSD)

This information applies to the CompactLogix 5380P and ControlLogix 5580P controllers.
The Process Variable Speed Drive (PVSD) instruction monitors and controls a variable speed motor using an AC (variable frequency) or DC drive. Use the instruction to run or jog the motor, forward or reverse. The drive interface can be through a Device Object Interface or through individual pins. The object is a built-in version of the existing P_VSD add-on instruction in the Rockwell Automation Library of Process Objects.
Use the PVSD instruction to:
  • Control and monitor a variable speed motor using an AC or DC drive. This instruction is used with drives controlling velocity, not position, and it does not use any motion axes.
  • Select Operator, Program, External, Override, Maintenance, Out of Service, or Hand as the source of drive commands and settings.
  • Use the selected command source to enter a speed reference (setpoint).
  • Use the selected command source to start the drive forward.
  • Use the selected command source to start the drive reverse, if configured for reversing.
  • Use the selected command source to jog the drive forward, if configured for jogging forward. Only Operator, External and Maintenance command sources are permitted to jog the drive forward.
  • Use the selected command source to jog the drive reverse, if configured for jogging reverse. Only Operator, External and Maintenance command sources are permitted to jog the drive reverse.
  • Monitor actual drive status, including:
    • Speed feedback
    • Drive ready
    • Drive active (run feedback)
    • Commanded direction
    • Actual direction
    • Accelerating
    • Decelerating
    • At speed
    • Drive warning
    • Drive faulted (with fault code and description)
  • Interface to a drive Device Object using a set of Power Velocity interface tags. If the interface tags are not linked (optional InOut parameters), a set of input and output parameters are used to interface to the drive signal-by-signal.
  • Search a linked Fault Code Lookup Table to provide textual drive fault information, or use text provided through the Power Velocity interface fault record.
  • Participate in a control strategy bus (BUS_OBJ) with other devices and process instructions.
  • Configure an output to provide a pre-start audible warning (horn). The time the alert sounds before starting or jogging is configurable.
  • Configure virtualization, providing simulated feedback of a working drive while disabling outputs to the physical device.
  • Configure scaling of the speed reference from application engineering units to drive interface units.
  • Configure scaling of the speed feedback from drive interface units to application engineering units.
  • Configure limiting (clamping) of the speed reference.
  • Monitor run feedback and provide status and alarms for failure to start in the configured time and failure to stop in the configured time.
  • Monitor permissive conditions to allow starting or jogging the motor forward.
  • Monitor permissive conditions to allow starting or jogging the motor reverse.
  • Monitor interlock conditions to stop and prevent starting or jogging the motor. Trigger an alarm if interlock conditions cause the motor to stop.
  • Monitor I/O communication faults.
  • Automatically clear latched alarms and drive faults when an Operator Command (Start, Stop, Jog) is received.
  • Automatically clear latched alarms and drive faults when an External Command (Start, Stop, Jog) is received.
  • Use HMI breadcrumbs for Alarm Inhibited, Bad Configuration, Not Ready, and Maintenance Bypass Active.
  • Use Available status for use by automation logic to indicate whether the motor can be controlled by other objects.
  • Use Alarms for Fail to Start, Fail to Stop, Interlock Trip, I/O Fault and Drive Fault conditions.
Available Languages
Ladder Diagram
PVSD_avail_ladder
Function Block Diagram
PVSD_avail_FBD
Structured Text
PVSD(
PlantPAx Control
, Ref_Ctrl_Set, Ref_Ctrl_Cmd, Ref_Ctrl_Sts, BusObj, Ref_FaultCodeList)
Operands
IMPORTANT:
Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand
Type
Format
Description
PlantPAx Control
P_VARIABLE_SPEED_DRIVE
tag
Data structure required for proper operation of instruction.
Ref_Ctrl_Set
RAC_ITF_DVC_PWRVELOCITY_SET
tag
Velocity Automation Device Object Settings Interface.
Ref_Ctrl_Cmd
RAC_ITF_DVC_PWRVELOCITY_CMD
tag
Velocity Automation Device Object Command Interface.
Ref_Ctrl_Sts
RAC_ITF_DVC_PWRVELOCITY_STS
tag
Velocity Automation Device Object Status Interface.
BusObj
BUS_OBJ
tag
Bus component.
Ref_FaultCodeList
RAC_CODE_DESCRIPTION[x]
tag
Fault Code to Fault Description lookup table for intelligent motor controller.
P_VARIABLE_SPEED_DRIVE Structure
Public members are standard, visible tag members that are programmatically accessible. Private, hidden members are used in HMI faceplates and are not programmatically accessible. Private members are listed in separate tables after public members.
Public Input Members
Data Type
FBD Default Visibility
FBD Wiring required
Usage
Description
EnableIn
BOOL
Not Visible
Not Required
Input
Enable Input - System Defined Parameter
Default is true.
Inp_InitializeReq
BOOL
Not Visible
Not Required
Input
1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request when reinitialization is needed. The instruction clears this operand automatically.
Default is true.
Inp_OwnerCmd
DINT
Not Visible
Not Required
Input
Owner device command.
0 = None,
.10 = Operator Lock,
.11 = Operator Unlock,
.12 = Program Lock,
.13 = Program Unlock,
.14 = Acquire Maintenance,
.15 = Release Maintenance,
.16 = Acquire External,
.17 = Release External,
.29 = Echo.
Default is 0.
Inp_SpeedFdbkData
REAL
Not Visible
Not Required
Input
Speed feedback in drive (raw) units (example: 0 to 32767 in drive units represents 0 to max frequency).
Default is 0.0.
Inp_DatalinkData
REAL
Not Visible
Not Required
Input
Auxiliary signal (datalink) input in drive (raw) units.
Default is 0.0.
Inp_LastFaultCodeData
DINT
Not Visible
Not Required
Input
Most recent drive fault code (enumeration).
Default is 0.
Inp_ReadyData
BOOL
Not Visible
Not Required
Input
1 = Drive is ready to run.
Default is true.
Inp_RunningData
BOOL
Not Visible
Not Required
Input
1 = Drive is running (active).
Default is false.
Inp_CommandDirData
BOOL
Not Visible
Not Required
Input
1 = Drive is commanded forward, 0 = drive is commanded reverse.
Default is true.
Inp_ActualDirData
BOOL
Not Visible
Not Required
Input
1 = Drive is running forward, 0 = drive is running reverse.
Default is true.
Inp_AcceleratingData
BOOL
Not Visible
Not Required
Input
1 = Drive is accelerating.
Default is false.
Inp_DeceleratingData
BOOL
Not Visible
Not Required
Input
1 = Drive is decelerating.
Default is false.
Inp_AtSpeedData
BOOL
Not Visible
Not Required
Input
1 = Drive is at commanded speed.
Default is false.
Inp_AlarmData
BOOL
Not Visible
Not Required
Input
1 = Drive has an alarm (warning) condition. See drive display or manual for detail.
Default is false.
Inp_FaultedData
BOOL
Not Visible
Not Required
Input
1 = Drive has faulted. See drive display or manual for detail.
Default is false.
Inp_DvcNotify
SINT
Not Visible
Not Required
Input
Related device object alarm priority and acknowledgement status.
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Inp_IOFault
BOOL
Visible
Not Required
Input
Indicates the IO data are inaccurate.
0 = The IO data are good, 1 = The IO data are bad, causing fault. If the drive is not virtual, this input sets Sts_IOFault, which raises IOFault Alarm.
Default is false.
Inp_FwdPermOK
BOOL
Visible
Not Required
Input
1 = Permissives OK, drive can start or jog forward.
Default is true.
Inp_FwdNBPermOK
BOOL
Visible
Not Required
Input
1 = Non-Bypassable Permissives OK, drive can start or jog forward.
Default is true.
Inp_RevPermOK
BOOL
Visible
Not Required
Input
1 = Permissives OK, drive can start or jog reverse.
Default is true.
Inp_RevNBPermOK
BOOL
Visible
Not Required
Input
1 = Non-Bypassable Permissives OK, drive can start or jog reverse.
Default is true.
Inp_IntlkOK
BOOL
Visible
Not Required
Input
1 = Interlocks OK, drive can start or jog and keep running.
Default is true.
Inp_NBIntlkOK
BOOL
Visible
Not Required
Input
1 = Non-bypassable interlocks OK, drive can start or jog and keep running.
Default is true.
Inp_IntlkAvailable
BOOL
Visible
Not Required
Input
1 = Interlock Availibility OK.
Default is false.
Inp_IntlkTripInh
BOOL
Visible
Not Required
Input
1 = Inhibit Interlock Trip Status.
Default is false.
Inp_RdyReset
BOOL
Not Visible
Not Required
Input
1 = Related object, reset by this object, is ready to be reset.
Default is false.
Inp_Hand
BOOL
Not Visible
Not Required
Input
1 = Acquire Hand (typically hardwired local), 0 = Release Hand.
Default is false.
Inp_Ovrd
BOOL
Not Visible
Not Required
Input
1 = Acquire Override (higher priority program logic), 0 = Release Override.
Default is false.
Inp_OvrdCmd
SINT
Not Visible
Not Required
Input
Override Command:
0 = None,
1 = Stop,
2 = Start Forward,
3 = Start Reverse.
Default is 0.
Inp_OvrdSpeed
REAL
Not Visible
Not Required
Input
Value to set Speed Reference in Override, in speed reference engineering units.
Default is 0.0.
Inp_OvrdOutDatalink
REAL
Not Visible
Not Required
Input
Value to set Output Datalink in Override, in output datalink engineering units.
Default is 0.0.
Inp_ExtInh
BOOL
Not Visible
Not Required
Input
1 = Inhibit External acquisition, 0 = Allow External acquisition.
Default is false.
Inp_HornInh
BOOL
Not Visible
Not Required
Input
1 = Inhibit audible alert, 0 = Alllow audible alert.
Default is false.
Inp_Reset
BOOL
Not Visible
Not Required
Input
1 = Reset Shed Latches and Cleared Alarms.
Default is false.
Cfg_AllowDisable
BOOL
Not Visible
Not Required
Input
1 = Allow Maintenance to disable alarms.
Default is true.
Cfg_AllowShelve
BOOL
Not Visible
Not Required
Input
1 = Allow Operator to shelve alarms.
Default is true.
Cfg_HasReverse
BOOL
Not Visible
Not Required
Input
1 = Drive can run or jog reverse, 0 = only allow forward operation.
Default is false.
Cfg_HasJog
BOOL
Not Visible
Not Required
Input
1 = Drive jog command enabled and visible, 0 = drive jog command not allowed.
Default is false.
Cfg_AllowLocal
BOOL
Not Visible
Not Required
Input
1 = Allow Local Start and Stop without alarm, 0 = Start or Stop by command only.
Default is false.
Cfg_HasRunFdbk
BOOL
Not Visible
Not Required
Input
1 = Drive provides feedback signal when running.
Default is false.
Cfg_UseRunFdbk
BOOL
Not Visible
Not Required
Input
1 = Drive run feedback should be used for failure checking.
Default is false.
Cfg_HasSpeedFdbk
BOOL
Not Visible
Not Required
Input
1 = Drive provides speed feedback.
Default is false.
Cfg_UseSpeedFdbk
BOOL
Not Visible
Not Required
Input
1 = Drive speed determines running state, 0 = state determined by drive active feedback.
Default is false.
Cfg_HasInpDatalink
BOOL
Not Visible
Not Required
Input
1 = A signal is connected to Inp_DatalinkData.
Default is false.
Cfg_HasOutDatalink
BOOL
Not Visible
Not Required
Input
1 = A signal is connected to Out_DatalinkData.
Default is false.
Cfg_HasDvcObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI a device (e.g., drive) object is connected.
Default is false.
Cfg_HasFwdPermObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI an object is connected to forward permissive inputs.
Default is false.
Cfg_HasRevPermObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI an object is connected to reverse permissive inputs.
Default is false.
Cfg_HasIntlkObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI an object is connected to interlock inputs.
Default is false.
Cfg_HasResInhObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI a Restart Inhibit object is connected.
Default is false.
Cfg_HasRunTimeObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI a Run Time / Starts object is connected.
Default is false.
Cfg_HasMoreObj
BOOL
Not Visible
Not Required
Input
1 = Tells HMI an object with more information is available.
Default is false.
Cfg_SetTrack
BOOL
Not Visible
Not Required
Input
1 = Settings track for unselected sources, 0 = no tracking of settings.
Default is true.
Cfg_SetTrackOvrdHand
BOOL
Not Visible
Not Required
Input
1 = Program, Operator and External settings track when Override or Hand is selected.
Default is false.
Cfg_OperStopPrio
BOOL
Not Visible
Not Required
Input
1 = OCmd_Stop accepted any time;
0 = OCmd_Stop accepted only when Oper is selected.
Default is false.
Cfg_ExtStopPrio
BOOL
Not Visible
Not Required
Input
1 = XCmd_Stop accepted any time;
0 = XCmd_Stop accepted only when Ext is selected.
Default is false.
Cfg_OCmdResets
BOOL
Not Visible
Not Required
Input
1 = Any drive OCmd resets shed latches and cleared alarms;
0 = OCmdReset is required.
Default is false.
Cfg_XCmdResets
BOOL
Not Visible
Not Required
Input
1 = Any drive XCmd resets shed latches and cleared alarms;
0 = XCmdReset is required.
Default is false.
Cfg_OvrdPermIntlk
BOOL
Not Visible
Not Required
Input
1 = Override ignores Bypassable Perm/ Intlk; 0 = Override uses all Perm/Intlk.
Default is false.
Cfg_ShedOnFailToStart
BOOL
Not Visible
Not Required
Input
1 = Stop Motor and Alarm on Fail to Start; 0 = Alarm only on Fail to Start.
Default is true.
Cfg_ShedOnIOFault
BOOL
Not Visible
Not Required
Input
1 = Stop Motor and Alarm on I/O Fault; 0 = Alarm only on I/O Fault.
Default is true.
Cfg_HasOper
BOOL
Not Visible
Not Required
Input
1 = Operator (unlocked) exists, can be selected.
Default is true.
Cfg_HasOperLocked
BOOL
Not Visible
Not Required
Input
1 = Operator Locked exists, can be selected.
Default is true.
Cfg_HasProg
BOOL
Not Visible
Not Required
Input
1 = Program (unlocked) exists, can be selected.
Default is true.
Cfg_HasProgLocked
BOOL
Not Visible
Not Required
Input
1 = Program Locked exists, can be selected.
Default is true.
Cfg_HasExt
BOOL
Not Visible
Not Required
Input
1 = External exists, can be selected.
Default is false.
Cfg_HasMaint
BOOL
Not Visible
Not Required
Input
1 = Maintenance exists, can be selected.
Default is true.
Cfg_HasMaintOoS
BOOL
Not Visible
Not Required
Input
1 = Maintenance Out of Service exists, can be selected.
Default is true.
Cfg_OvrdOverLock
BOOL
Not Visible
Not Required
Input
1 = Override supersedes Program/Operator Lock, 0 = Don't override Lock.
Default is true.
Cfg_ExtOverLock
BOOL
Not Visible
Not Required
Input
1 = External supersedes Program/Operator Lock, 0 = Don't override Lock.
Default is false.
Cfg_ProgPwrUp
BOOL
Not Visible
Not Required
Input
1 = Power up to Program, 0 = Power up to Operator.
Default is false.
Cfg_ProgNormal
BOOL
Not Visible
Not Required
Input
Normal Source: 1 = Program if no requests; 0 = Operator if no requests.
Default is false.
Cfg_PCmdPriority
BOOL
Not Visible
Not Required
Input
Command priority. 1 = Program commands win, 0 = Operator commands win.
Default is false.
Cfg_PCmdProgAsLevel
BOOL
Not Visible
Not Required
Input
1 = PCmd_Prog used as a Level (1 = Prog, 0 = Oper).
Default is false.
Cfg_PCmdLockAsLevel
BOOL
Not Visible
Not Required
Input
1 = PCmd_Lock used as a Level (1 = Lock, 0 = Unlock).
Default is false.
Cfg_ExtAcqAsLevel
BOOL
Not Visible
Not Required
Input
1 = XCmd_Acq used as Level (1 = Acquire, 0 = Release).
Default is false.
Cfg_DecPlcs
SINT
Not Visible
Not Required
Input
Number of decimal places for speed ref/fdbk display (0 to 6).
Default is 2.
Cfg_InpDatalinkDecPlcs
SINT
Not Visible
Not Required
Input
Number of decimal places for Input Datalink display (0 to 6).
Default is 2.
Cfg_OutDatalinkDecPlcs
SINT
Not Visible
Not Required
Input
Number of decimal places for Output Datalink display (0 to 6).
Default is 2.
Cfg_MinSpeedRef
REAL
Not Visible
Not Required
Input
Minimum Speed Reference in EU (for limiting). Valid = any float less than or equal to Cfg_MaxSpeedRef and greater than or equal to Cfg_SpeedRefEUMin.
Default is 0.0.
Cfg_MaxSpeedRef
REAL
Not Visible
Not Required
Input
Maximum Speed Reference in EU (for limiting). Valid = any float greater than or equal to Cfg_MinSpeedRef and less than or equal to Cfg_SpeedRefEUMax.
Default is 60.0.
Cfg_JogSpeedRef
REAL
Not Visible
Not Required
Input
Speed Reference to use when Jogging (EU). Valid = any float (will be clamped at configured Min and Max).
Default is 10.0.
Cfg_SpeedRefRawMin
REAL
Not Visible
Not Required
Input
Speed Reference Minimum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_SpeedRefRawMax.
Default is 0.0.
Cfg_SpeedRefRawMax
REAL
Not Visible
Not Required
Input
Speed Reference Maximum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_SpeedRefRawMin.
Default is 60.0.
Cfg_SpeedRefEUMin
REAL
Not Visible
Not Required
Input
Speed Reference Minimum in Engineering Units (for scaling). Valid = any float less than Cfg_SpeedRefEUMax.
Default is 0.0.
Cfg_SpeedRefEUMax
REAL
Not Visible
Not Required
Input
Speed Reference Maximum in Engineering Units (for scaling). Valid = any float greater than Cfg_SpeedRefEUMin.
Default is 60.0.
Cfg_SpeedFdbkRawMin
REAL
Not Visible
Not Required
Input
Speed Feedback Minimum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_SpeedFdbkRawMax.
Default is 0.0.
Cfg_SpeedFdbkRawMax
REAL
Not Visible
Not Required
Input
Speed Feedback Maximum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_SpeedFdbkRawMin.
Default is 60.0.
Cfg_SpeedFdbkEUMin
REAL
Not Visible
Not Required
Input
Speed Feedback Minimum in Engineering Units (for scaling). Valid = any float less than Cfg_SpeedFdbkEUMax.
Default is 0.0.
Cfg_SpeedFdbkEUMax
REAL
Not Visible
Not Required
Input
Speed Feedback Maximum in Engineering Units (for scaling). Valid = any float greater than Cfg_SpeedFdbkEUMin.
Default is 60.0.
Cfg_InpDatalinkRawMin
REAL
Not Visible
Not Required
Input
Input Datalink Minimum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_InpDatalinkRawMax.
Default is 0.0.
Cfg_InpDatalinkRawMax
REAL
Not Visible
Not Required
Input
Input Datalink Maximum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_InpDatalinkRawMin.
Default is 100.0.
Cfg_InpDatalinkEUMin
REAL
Not Visible
Not Required
Input
Input Datalink Minimum in Engineering Units (for scaling). Valid = any float less than Cfg_InpDatalinkEUMax.
Default is 0.0.
Cfg_InpDatalinkEUMax
REAL
Not Visible
Not Required
Input
Input Datalink Maximum in Engineering Units (for scaling). Valid = any float greater than Cfg_InpDatalinkEUMin.
Default is 100.0.
Cfg_OutDatalinkMin
REAL
Not Visible
Not Required
Input
Minimum Output Datalink in EU (for limiting). Valid = any float less than or equal to Cfg_OutDatalinkMax and greater than or equal to Cfg_OutDatalinkEUMin.
Default is 0.0.
Cfg_OutDatalinkMax
REAL
Not Visible
Not Required
Input
Maximum Output Datalink in EU (for limiting). Valid = any float greater than or equal to Cfg_OutDatalinkMin and less than or equal to Cfg_OutDatalinkEUMax.
Default is 100.0.
Cfg_OutDatalinkRawMin
REAL
Not Visible
Not Required
Input
Output Datalink Minimum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_OutDatalinkRawMax.
Default is 0.0.
Cfg_OutDatalinkRawMax
REAL
Not Visible
Not Required
Input
Output Datalink Maximum in Drive (raw) Units (for scaling). Valid = any float not equal to Cfg_OutDatalinkRawMin.
Default is 100.0.
Cfg_OutDatalinkEUMin
REAL
Not Visible
Not Required
Input
Output Datalink Minimum in Engineering Units (for scaling). Valid = any float less than Cfg_OutDatalinkEUMax.
Default is 0.0.
Cfg_OutDatalinkEUMax
REAL
Not Visible
Not Required
Input
Output Datalink Maximum in Engineering Units (for scaling). Valid = any float greater than Cfg_OutDatalinkEUMin.
Default is 100.0.
Cfg_StartHornTime
REAL
Not Visible
Not Required
Input
Time in seconds to sound audible on commanded start. Valid = 0.0 to 1000.0 seconds, 0.0 = disabled.
Default is 0.0.
Cfg_VirtualRampTime
REAL
Not Visible
Not Required
Input
Time in seconds to ramp speed feedback when Virtualized. Valid = 0.0 to max float.
Default is 10.0.
Cfg_FailToStartTime
REAL
Not Visible
Not Required
Input
Time in seconds after Start to receive Run Feedback before Fault. Valid = 0.0 to 2147483.0 seconds.
Default is 15.0.
Cfg_FailToStopTime
REAL
Not Visible
Not Required
Input
Time in seconds after Stop to drop Run Feedback before Fault. Valid = 0.0 to 2147483,0 seconds.
Default is 15.0.
Cfg_ResetPulseTime
REAL
Not Visible
Not Required
Input
Time in seconds to pulse Out_Reset to clear Motor fault. Valid = 0.0 to 2147483.0 seconds.
Default is 2.0.
Cfg_MaxJogTime
REAL
Not Visible
Not Required
Input
Maximum jog time in seconds. Valid = 0.0 to 2147483.0 seconds, 0.0 = unlimited).
Default is 0.0.
Cfg_eKeepRef
SINT
Not Visible
Not Required
Input
Ownership of Speed Reference (enumeration):
0 = follows CmdSrc,
1 = Operator,
2 = Program,
3 = External.
Default is 0.
Cfg_eKeepStart
SINT
Not Visible
Not Required
Input
Ownership of Start commands (enumeration):
0 = follows CmdSrc,
1 = Operator,
2 = Program,
3 = External.
Default is 0.
Cfg_eKeepJog
SINT
Not Visible
Not Required
Input
Ownership of Jog commands (enumeration):
0 = follows CmdSrc,
1 = Operator,
3 = External.
Default is 0.
Cfg_eKeepOutDatalink
SINT
Not Visible
Not Required
Input
Ownership of Output Datalink (enumeration):
0 = follows CmdSrc,
1 = Operator,
2 = Program,
3 = External.
Default is 0.
Cfg_CnfrmReqd
SINT
Not Visible
Not Required
Input
Operator Command Confirmation Required. Represents the type of command confirmation required.
0 = None,
1 = Command confirmation required,
2 = Performer e-signature required,
3 = Performer and approver e-signature required.
Default is 0.
Cfg_HasHistTrend
SINT
Not Visible
Not Required
Input
Has Historical Trend. This enables navigation to the Device Historical Trend Faceplate from the HMI.
0 = No external historical trend,
1 = Datalog historical trend,
2 = Historian historical trend.
Default is 0.
PSet_SpeedRef
REAL
Not Visible
Not Required
Input
Program Setting of Run Speed Reference (speed reference engineering units). Valid = any real, will be clamped.
Default is 0.0.
PSet_OutDatalink
REAL
Not Visible
Not Required
Input
Program Setting of Output Datalink (output datalink engineering units). Valid = any real, will be clamped.
Default is 0.0.
PSet_Owner
DINT
Not Visible
Not Required
Input
Program owner request ID (non-zero) or release (zero).
Default is 0.
XSet_SpeedRef
REAL
Not Visible
Not Required
Input
External setting of Run Speed Reference (speed reference engineering units). Valid = any real, will be clamped.
Default is 0.0.
XSet_OutDatalink
REAL
Not Visible
Not Required
Input
External setting of Output Datalink (output datalink engineering units). Valid = any real, will be clamped.
Default is 0.0.
PCmd_Virtual
BOOL
Not Visible
Not Required
Input
Program command to select Virtual (simulated) device operation. The instruction clears this operand automatically.
Default is false.
PCmd_Physical
BOOL
Not Visible
Not Required
Input
Program command to select Physical device operation (not simulated). The instruction clears this operand automatically.
Default is false.
PCmd_StartFwd
BOOL
Not Visible
Not Required
Input
Program command to Start Drive Forward. The instruction clears this operand automatically.
Default is false.
PCmd_StartRev
BOOL
Not Visible
Not Required
Input
Program command to Start Drive Reverse. The instruction clears this operand automatically.
Default is false.
PCmd_Stop
BOOL
Not Visible
Not Required
Input
Program command to Stop Drive. The instruction clears this operand automatically.
Default is false.
PCmd_Prog
BOOL
Not Visible
Not Required
Input
Program command to select Program (Operator to Program). The instruction clears this operand automatically if Cfg_PCmdProgAsLevel = 0.
Default is false.
PCmd_Oper
BOOL
Not Visible
Not Required
Input
Program command to select Operator (Program to Operator). The instruction clears this operand automatically.
Default is false.
PCmd_Lock
BOOL
Not Visible
Not Required
Input
Program command to lock Program (disallow Operator). The instruction clears this operand automatically if Cfg_PCmdLockAsLevel = 0.
Default is false.
PCmd_Unlock
BOOL
Not Visible
Not Required
Input
Program command to unlock Program (allow Operator to acquire). The instruction clears this operand automatically.
Default is false.
PCmd_Normal
BOOL
Not Visible
Not Required
Input
Program command to select Normal command source (Operator or Program). The instruction clears this operand automatically.
Default is false.
PCmd_Reset
BOOL
Not Visible
Not Required
Input
Program command to reset all alarms and latched shed conditions requiring reset. The instruction clears this operand automatically.
Default is false.
MCmd_Rel
BOOL
Not Visible
Not Required
Input
Maintenance command to release ownership (Maintenance to Operator/Program/External/Override). The instruction clears this operand automatically.
Default is false.
OCmd_Unlock
BOOL
Not Visible
Not Required
Input
Operator command to unlock / release (allow Program to acquire) ownership. The instruction clears this operand automatically.
Default is false.
XCmd_StartFwd
BOOL
Not Visible
Not Required
Input
External command to Start Drive Forward. The instruction clears this operand automatically.
Default is false.
XCmd_StartRev
BOOL
Not Visible
Not Required
Input
External command to Start Drive Reverse. The instruction clears this operand automatically.
Default is false.
XCmd_Stop
BOOL
Not Visible
Not Required
Input
External command to Stop Drive. The instruction clears this operand automatically.
Default is false.
XCmd_JogFwd
BOOL
Not Visible
Not Required
Input
External command to Jog Drive Forward. The instruction clears this operand automatically if max jog time is reached.
Default is false.
XCmd_JogRev
BOOL
Not Visible
Not Required
Input
External command to Jog Drive Reverse. The instruction clears this operand automatically if max jog time is reached..
Default is false.
XCmd_Acq
BOOL
Not Visible
Not Required
Input
External command to acquire ownership (Operator/Program/Override/Maintenance to External). The instruction clears this operand automatically if Cfg_ExtAcqAsLevel = 0.
Default is false.
XCmd_Rel
BOOL
Not Visible
Not Required
Input
External command to release ownership if Cfg_ExtAcqAsLevel = 0 (External to Operator/Program/Override/Maintenance). The instruction clears this operand automatically.
Default is false.
XCmd_Reset
BOOL
Not Visible
Not Required
Input
External command to clear shed latches and cleared alarms. The instruction clears this operand automatically.
Default is false.
XCmd_ResetAckAll
BOOL
Not Visible
Not Required
Input
External command to acknowledge and reset all alarms and latched shed conditions. The instruction clears this operand automatically.
Default is false.
Public Output Members
Data Type
FBD Default Visibility
FBD Wiring required
Usage
Description
EnableOut
BOOL
Not Visible
Not Required
Output
Enable Output - System Defined Parameter
Out_SpeedRefData
REAL
Not Visible
Not Required
Output
Speed reference in drive (raw) units (example: 0 to 32767 in drive units represents 0 to max frequency).
Out_DatalinkData
REAL
Not Visible
Not Required
Output
Auxiliary signal (datalink) output in drive (raw) units.
Out_RunData
BOOL
Not Visible
Not Required
Output
1 = Start/Run Drive, 0 = Stop Drive (for held starter type).
Out_StopData
BOOL
Not Visible
Not Required
Output
1 = Stop Drive, 0 = drive left in current state.
Out_StartData
BOOL
Not Visible
Not Required
Output
1 = Start Drive, 0 = drive left in current state.
Out_ClearFaultData
BOOL
Not Visible
Not Required
Output
1 = Attempt to clear Drive Fault.
Out_FwdData
BOOL
Not Visible
Not Required
Output
1 = Set drive direction to Forward.
Out_RevData
BOOL
Not Visible
Not Required
Output
1 = Set drive direction to Reverse.
Out_HornData
BOOL
Not Visible
Not Required
Output
1 = Sound audible prior to commanded motor start.
Out_Reset
BOOL
Not Visible
Not Required
Output
1 = Reset command has been received and accepted.
Out_OwnerSts
DINT
Not Visible
Not Required
Output
Status of command source, owner command handshake and ready status.
0 = None,
.10 = Operator Lock,
.11 = Operator Unlock,
.12 = Program Lock,
.13 = Program Unlock,
.14 = Acquire Maintenance,
.15 = Release Maintenance,
.16 = Acquire External,
.17 = Release External,
.18 = Has Maintenance,
.19 = External Override Lock,
.20 = Has External,
.21 = Has Operator,
.22 = Has Operator Locked,
.23 = Has Program,
.24 = Has Program Locked,
.29 = Echo,
.30 = Not Ready.
Val_SpeedRef
REAL
Visible
Not Required
Output
Speed Reference (target) to drive.
Val_SpeedFdbk
REAL
Visible
Not Required
Output
Speed Feedback (actual) from drive.
Val_InpDatalink
REAL
Not Visible
Not Required
Output
Input Datalink value from drive.
Val_OutDatalink
REAL
Not Visible
Not Required
Output
Output Datalink value to drive.
Val_SpeedRefEUMin
REAL
Not Visible
Not Required
Output
Minimum of Speed Reference = MIN (Cfg_SpeedFdbkEUMin, Cfg_SpeedFdbkEUMax).
Val_SpeedRefEUMax
REAL
Not Visible
Not Required
Output
Maximum of Speed Reference = MAX (Cfg_SpeedFdbkEUMin, Cfg_SpeedFdbkEUMax).
Val_SpeedFdbkEUMin
REAL
Not Visible
Not Required
Output
Minimum of Speed Feedback = MIN (Cfg_SpeedFdbkEUMin, Cfg_SpeedFdbkEUMax).
Val_SpeedFdbkEUMax
REAL
Not Visible
Not Required
Output
Maximum of Speed Feedback = MAX (Cfg_SpeedFdbkEUMin, Cfg_SpeedFdbkEUMax).
Sts_Initialized
BOOL
Not Visible
Not Required
Output
1 = Instruction is initialized. Use Inp_InitializeReq to reinitialize.
Sts_Stopped
BOOL
Visible
Not Required
Output
1 = Drive requested to stop and is confirmed stopped.
Sts_StartingFwd
BOOL
Visible
Not Required
Output
1 = Drive requested to run forward and awaiting run feedback.
Sts_StartingRev
BOOL
Not Visible
Not Required
Output
1 = Drive requested to run reverse and awaiting run feedback.
Sts_RunningFwd
BOOL
Visible
Not Required
Output
1 = Drive requested to run and is confirmed running forward.
Sts_RunningRev
BOOL
Not Visible
Not Required
Output
1 = Drive requested to run and is confirmed running reverse.
Sts_StoppingFwd
BOOL
Visible
Not Required
Output
1 = Drive running forward requested to stop and awaiting stopped feedback.
Sts_StoppingRev
BOOL
Not Visible
Not Required
Output
1 = Drive running reverse requested to stop and awaiting stopped feedback.
Sts_JoggingFwd
BOOL
Visible
Not Required
Output
1 = Drive requested to Jog Forward.
Sts_JoggingRev
BOOL
Not Visible
Not Required
Output
1 = Drive requested to Jog Reverse.
Sts_Horn
BOOL
Not Visible
Not Required
Output
1 = Motor Audible Alert (Horn) is Active.
Sts_CommandDir
BOOL
Not Visible
Not Required
Output
1 = Drive commanded to Forward, 0 = Reverse.
Sts_ActualDir
BOOL
Not Visible
Not Required
Output
1 = Motor rotation (actual direction) is Forward, 0 = Reverse.
Sts_Accel
BOOL
Not Visible
Not Required
Output
1 = Drive is Accelerating.
Sts_Decel
BOOL
Not Visible
Not Required
Output
1 = Drive is Decelerating.
Sts_NotReady
BOOL
Not Visible
Not Required
Output
1 = Drive is Not Ready (cannot be started) Check alarms, stops, faults.
Sts_Alarm
BOOL
Not Visible
Not Required
Output
1 = Drive has an Alarm (see drive display or manual).
Sts_AtSpeed
BOOL
Not Visible
Not Required
Output
1 = Drive is running at reference speed.
Sts_SpeedLimited
BOOL
Not Visible
Not Required
Output
1 = Speed Reference Setting exceeds configured Max/Min limit.
Sts_Virtual
BOOL
Not Visible
Not Required
Output
1 = The instruction treats the drive as virtual. The instruction acts as normal but the output is kept de-energized; 0 = The instruction operates the drive normally. Sts_Virtual is a copy of Sts_Virtual.
SrcQ_IO
SINT
Not Visible
Not Required
Output
Source and quality of primary input or output (enumerated):
0=Good, live, confirmed good
1=Good, live, assumed good
2=Good, no feedback, assumed good
8=Test, virtualized
9=Test, loopback
10=Test, manually entered
16=Uncertain, live, off-spec
17=Uncertain, substituted at device or bus
18=Uncertain, substituted at instruction
19=Uncertain, using last known good
20=Uncertain, using replacement value
32=Bad, signal failure
33=Bad, channel fault
34=Bad, module or communication fault
35=Bad, invalid configuration
SrcQ
SINT
Not Visible
Not Required
Output
Source and quality of primary value or status (enumerated):
0=Good, live, confirmed good
1=Good, live, assumed good
2=Good, no feedback, assumed good
8=Test, virtualized
9=Test, loopback
10=Test, manually entered
16=Uncertain, live, off-spec
17=Uncertain, substituted at device or bus
18=Uncertain, substituted at instruction
19=Uncertain, using last known good
20=Uncertain, using replacement value
32=Bad, signal failure
33=Bad, channel fault
34=Bad, module or communication fault
35=Bad, invalid configuration
Sts_eCmd
SINT
Not Visible
Not Required
Output
Drive Command:
0 = None,
1 = Stop,
2 = Start Forward,
3 = Start Reverse,
4 = Jog Forward,
5 = Jog Reverse.
Sts_eFdbk
SINT
Not Visible
Not Required
Output
Drive Feedback:
0 = Stopped,
1 = Running Forward,
2 = Running Reverse,
3 = Accelerating,
4 = Decelerating.
Sts_eSts
SINT
Not Visible
Not Required
Output
Drive Status:
0 = Powerup / Unknown,
1 = Stopped,
2 = Running Forward,
3 = Running Reverse,
4 = Starting Forward,
5 = Starting Reverse,
6 = Jogging Forward,
7 = Jogging Reverse,
8 = Stopping,
14 = Horn,
15 = Out Of Service.
Sts_eFault
SINT
Not Visible
Not Required
Output
Drive Fault Status:
0 = None,
15 = Interlock Trip,
16 = Fail to Start,
17 = Fail to Stop,
18 = Drive Fault,
32 = I/O Fault,
34 = Config Error.
Sts_eNotify
SINT
Not Visible
Not Required
Output
All alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyAll
SINT
Not Visible
Not Required
Output
All alarm status enumerated values including related objects:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyIOFault
SINT
Not Visible
Not Required
Output
IOFault alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyFailToStart
SINT
Not Visible
Not Required
Output
Fail to Start alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyFailToStop
SINT
Not Visible
Not Required
Output
Fail to Stop alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyIntlkTrip
SINT
Not Visible
Not Required
Output
IntlkTrip alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowledged.
Sts_eNotifyDriveFault
SINT
Not Visible
Not Required
Output
Drive Fault alarm status enumerated values:
0 = Not in alarm, acknowledged,
1 = Not in alarm, unacknowledged or reset required,
2 = Low severity alarm, acknowledged,
3 = Low severity alarm, unacknowledged,
4 = Medium severity alarm, acknowledged,
5 = Medium severity alarm, unacknowledged,
6 = High severity alarm, acknowledged,
7 = High severity alarm, unacknowledged,
8 = Urgent severity alarm, acknowledged,
9 = Urgent severity alarm, unacknowl
Sts_UnackAlmCount
DINT
Not Visible
Not Required
Output
Count of unacknowledged alarms.
Sts_eFaultCode
DINT
Not Visible
Not Required
Output
First Drive Fault Code after reset. See drive manual or Drive Object for description.
Sts_eSrc
INT
Not Visible
Not Required
Output
The current command source is shown with status bits:
Sts_eSrc.0: Lock,
Sts_eSrc.1: Normal,
Sts_eSrc.2: Hand,
Sts_eSrc.3: Maintenance,
Sts_eSrc.4: Override,
Sts_eSrc.5: Program,
Sts_eSrc.6: Operator,
Sts_eSrc.7: Out of Service,
Sts_eSrc.8: External.
Sts_bSrc
INT
Not Visible
Not Required
Output
Active selection bitmap (for HMI totem pole with command source request selection):
Sts_bSrc.0: Hand,
Sts_bSrc.1: Programmed Out of Service (rung false),
Sts_bSrc.2: Maintenance Out of Service,
Sts_bSrc.3: Maintenance,
Sts_bSrc.4: Override,
Sts_bSrc.5: External,
Sts_bSrc.6: Program locked,
Sts_bSrc.7: Program,
Sts_bSrc.8: Operator locked,
Sts_bSrc.9: Operator.
Sts_Available
BOOL
Not Visible
Not Required
Output
1 = Device has been acquired by Program and is now available for start/stop control.
Sts_IntlkAvailable
BOOL
Not Visible
Not Required
Output
1 = Device can be acquired by Program and is available for start/stop control when interlocks are OK.
Sts_Bypass
BOOL
Not Visible
Not Required
Output
1 = Bypassable interlocks are bypassed.
Sts_BypActive
BOOL
Visible
Not Required
Output
1 = Interlock bypassing active (bypassed or maintenance).
Sts_MaintByp
BOOL
Not Visible
Not Required
Output
1 = Device has a maintenance bypass function active.
Sts_NotRdy
BOOL
Not Visible
Not Required
Output
1 = Device is not ready, see detail bits (Sts_Nrdyxxx) for reason.
Sts_NrdyCfgErr
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Configuration error.
Sts_NrdyDriveNotReady
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Drive Not Ready.
Sts_NrdyFail
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Device failure (Shed requires Reset).
Sts_NrdyIntlk
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Interlock not OK.
Sts_NrdyIOFault
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: IO Fault (Shed requires Reset).
Sts_NrdyOoS
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Device disabled by Maintenance.
Sts_NrdyFwdPerm
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Forward permissive not OK.
Sts_NrdyRevPerm
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Reverse permissive not OK.
Sts_NrdyPrioStop
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Operator or External priority Stop command requires reset.
Sts_NrdyTrip
BOOL
Not Visible
Not Required
Output
1 = Device is not ready: Device Tripped (Drive Fault requires Reset).
Sts_Err
BOOL
Visible
Not Required
Output
1 = Error in configuration: See detail bits (Sts_ErrXxx) for reason.
Sts_ErrAlm
BOOL
Not Visible
Not Required
Output
1 = Error in Logix tag-based alarm settings.
Sts_ErrSpeedFdbkRaw
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Speed Fdbk Raw Cfg_SpeedFdbkRawMin = Cfg_SpeedFdbkRawMax.
Sts_ErrSpeedFdbkEU
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_SpeedFdbkEUMax <= Cfg_SpeedFdbkEUMin.
Sts_ErrSpeedRefLim
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_MaxSpeedRef < Cfg_MinSpeedRef or Cfg_MaxSpeedRef > Cfg_SpeedRefEUMax or Cfg_MinSpeedRef < Cfg_SpeedRefEUMin.
Sts_ErrSpeedRefEU
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_SpeedRefEUMax <= Cfg_SpeedRefEUMin.
Sts_ErrSpeedRefRaw
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_SpeedRefRawMin = Cfg_SpeedRefRawMax.
Sts_ErrInpDatalinkRaw
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_InpDatalinkRawMin = Cfg_InpDatalinkRawMax.
Sts_ErrInpDatalinkEU
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_InpDataLinkEUMax <= Cfg_InpDatalinkEUMin.
Sts_ErrOutDatalinkLim
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_OutDatalinkMax < Cfg_OutDatalinkMin or Cfg_OutDatalinkMax > Cfg_OutDatalinkEUMax or Cfg_OutDatalinkMin < Cfg_OutDatalinkEUMin.
Sts_ErrOutDatalinkEU
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_OutDataLinkEUMax <= Cfg_OutDatalinkEUMin.
Sts_ErrOutDatalinkRaw
BOOL
Not Visible
Not Required
Output
1 = Error in configuration: Cfg_OutDatalinkRawMin = Cfg_OutDatalinkRawMax.
Sts_ErrVirtualRampTime
BOOL
Not Visible
Not Required
Output
1 = Error in Config: Virtual speed accel / decel time: use 0 to 2147483.
Sts_ErrFailToStartTime
BOOL
Not Visible
Not Required
Output
1 = Error in Config: Fail to Start timer preset: use 0 to 2147483.
Sts_ErrFailToStopTime
BOOL
Not Visible
Not Required
Output
1 = Error in Config: Fail to Stop timer preset: use 0 to 2147483.
Sts_ErrResetPulseTime
BOOL
Not Visible
Not Required
Output
1 = Error in Config: Reset Pulse timer preset: use 0 to 2147483.
Sts_ErrMaxJogTime
BOOL
Not Visible
Not Required
Output
1 = Error in Config: Maximum Jog Time timer preset: use 0 to 2147483.
Sts_Hand
BOOL
Visible
Not Required
Output
1 = Hand is selected (supersedes OoS, Maintenance, Override, External, Program, Operator).
Sts_OoS
BOOL
Visible
Not Required
Output
1 = Out of Service is selected (supersedes Maintenance, Override, External, Program, Operator).
Sts_Maint
BOOL
Visible
Not Required
Output
1 = Maintenance is selected (supersedes Override, External, Program, Operator).
Sts_Ovrd
BOOL
Visible
Not Required
Output
1 = Override is selected (supersedes External, Program, Operator).
Sts_Ext
BOOL
Visible
Not Required
Output
1 = External is selected (supersedes Program and Operator).
Sts_Prog
BOOL
Visible
Not Required
Output
1 = Program is selected.
Sts_ProgLocked
BOOL
Not Visible
Not Required
Output
1 = Program is selected and Locked.
Sts_Oper
BOOL
Visible
Not Required
Output
1 = Operator is selected.
Sts_OperLocked
BOOL
Not Visible
Not Required
Output
1 = Operator is selected and Locked.
Sts_ProgOperSel
BOOL
Not Visible
Not Required
Output
Program/Operator selection (latch) state: 1 = Program, 0 = Operator.
Sts_ProgOperLock
BOOL
Visible
Not Required
Output
Program/Operator lock (latch) state, 1 = Locked, 0 = Unlocked.
Sts_Normal
BOOL
Not Visible
Not Required
Output
1 = Selection equals the Normal (Program or Operator).
Sts_ExtReqInh
BOOL
Not Visible
Not Required
Output
1 = External request inhibited, cannot get to External from current state.
Sts_ProgReqInh
BOOL
Not Visible
Not Required
Output
1 = Program request inhibited, cannot get to Program from current state.
Sts_MAcqRcvd
BOOL
Not Visible
Not Required
Output
1 = Maintenance Acquire command received this scan.
Sts_CmdConflict
BOOL
Not Visible
Not Required
Output
1 = Conflicting commands received this scan.
Sts_Alm
BOOL
Not Visible
Not Required
Output
1 = An alarm is active.
Sts_AlmInh
BOOL
Not Visible
Not Required
Output
1 = An alarm is shelved or disabled.
Sts_IOFault
BOOL
Not Visible
Not Required
Output
IO Fault status: 1 = Bad, 0 = OK. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVSDTag.@Alarms.Alm_IOFault.AlarmElement.
Sts_FailToStart
BOOL
Not Visible
Not Required
Output
1 = Drive failed to Start. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVSDTag.@Alarms.Alm_FailToStart.AlarmElement.
Sts_FailToStop
BOOL
Not Visible
Not Required
Output
1 = Drive failed to Stop. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVSDTag.@Alarms.Alm_FailToStop.AlarmElement.
Sts_IntlkTrip
BOOL
Not Visible
Not Required
Output
1 = Drive stopped by an interlock Not OK. There is a predefined default discrete Logix tag-based alarm for the status. Set standard configuration members of the discrete Logix tag-based alarm. Alarm elements can be accessed as follows: PVSDTag.@Alarms.Alm_IntlkTrip.AlarmElement.
Sts_DriveFault
BOOL
Not Visible
Not Required
Output
1 = Drive Fault, see drive display or manual for detail.
Sts_RdyAck
BOOL
Not Visible
Not Required
Output
1 = An alarm is ready to be acknowledged.
Sts_RdyReset
BOOL
Not Visible
Not Required
Output
1 = A latched alarm or shed condition is ready to be reset.
XRdy_Acq
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_Acq, enable HMI button.
XRdy_Rel
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_Rel, enable HMI button.
XRdy_StartFwd
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_StartFwd, enable button.
XRdy_StartRev
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_StartRev, enable button.
XRdy_JogFwd
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_JogFwd, enable button.
XRdy_JogRev
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_JogRev, enable button.
XRdy_Stop
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_Stop, enable button.
XRdy_Reset
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_Reset, enable button.
XRdy_ResetAckAll
BOOL
Not Visible
Not Required
Output
1 = Ready for XCmd_ResetAckAll, enable button.
Val_Owner
DINT
Not Visible
Not Required
Output
Current object owner ID (0 = not owned).
Private Input Members
Data Type
Description
CmdSrc
P_COMMAND_SOURCE
Control or Command Source Selection.
MCmd_Acq
BOOL
Maintenance command to acquire ownership (Operator/Program/External/Override to Maintenance). The instruction clears this operand automatically.
Default is false.
MCmd_Bypass
BOOL
Maintenance command to bypass all bypassable interlocks and permissives. The instruction clears this operand automatically.
Default is false.
MCmd_Check
BOOL
Maintenance command to check (not bypass) all interlocks and permissives. The instruction clears this operand automatically.
Default is false.
MCmd_IS
BOOL
Maintenance command to select In Service. The instruction clears this operand automatically.
Default is false.
MCmd_OoS
BOOL
Maintenance command to select Out of Service. The instruction clears this operand automatically.
Default is false.
MCmd_Physical
BOOL
Maintenance command to select Physical device operation (not simulated). The instruction clears this operand automatically.
Default is false.
MCmd_Virtual
BOOL
Maintenance command to select Virtual (simulated) device operation. The instruction clears this operand automatically.
Default is false.
OCmd_JogFwd
BOOL
Operator command to Jog Drive Forward. The instruction clears this operand automatically if max jog time is reached.
Default is false.
OCmd_JogRev
BOOL
Operator command to Jog Drive Reverse. The instruction clears this operand automatically if max jog time is reached.
Default is false.
OCmd_Lock
BOOL
Operator command to lock Operator (disallow Program). The instruction clears this operand automatically.
Default is false.
OCmd_Normal
BOOL
Operator command to select Normal (Operator or Program). The instruction clears this operand automatically.
Default is false.
OCmd_Oper
BOOL
Operator command to select Operator (Program to Operator). The instruction clears this operand automatically.
Default is false.
OCmd_Prog
BOOL
Operator command to select Program (Operator to Program). The instruction clears this operand automatically.
Default is false.
OCmd_Reset
BOOL
Operator command to reset all alarms and latched shed conditions. The instruction clears this operand automatically.
Default is false.
OCmd_ResetAckAll
BOOL
Operator command to acknowledge and reset all alarms and latched shed conditions. The use of OCmd_ResetAckAll is restricted to HMI. The instruction clears this operand automatically.
Default is false.
OCmd_StartFwd
BOOL
Operator command to Start Drive Forward. The instruction clears this operand automatically.
Default is false.
OCmd_StartRev
BOOL
Operator command to Start Drive Reverse. The instruction clears this operand automatically.
Default is false.
OCmd_Stop
BOOL
Operator command to Stop Drive. The instruction clears this operand automatically.
Default is false.
OSet_OutDatalink
REAL
Operator Setting of Output Datalink, in output datalink engineering units. Valid = any float (clamped)
Default is 0.0.
OSet_SpeedRef
REAL
Operator Setting of Speed Reference, in speed reference engineering units. Valid = any float (clamped)
Default is 0.0.
Private Output Members
Data Type
Description
HMI_BusObjIndex
DINT
This object's index in the bus array, for use by HMI display.
Default is 0.
MRdy_Acq
BOOL
1 = Ready for MCmd_Acq, enable HMI button.
MRdy_Bypass
BOOL
1 = Ready for MCmd_Bypass, enable HMI button.
MRdy_Check
BOOL
1 = Ready for MCmd_Check, enable HMI button.
MRdy_IS
BOOL
1 = Ready for MCmd_IS, enable HMI button.
MRdy_OoS
BOOL
1 = Ready for MCmd_OoS, enable HMI button.
MRdy_Physical
BOOL
1 = Ready for MCmd_Physical, enable HMI button.
MRdy_Rel
BOOL
1 = Ready for MCmd_Rel, enable HMI button.
MRdy_Virtual
BOOL
1 = Ready for MCmd_Virtual, enable HMI button.
ORdy_JogFwd
BOOL
1 = Ready for OCmd_JogFwd, enable HMI button.
ORdy_JogRev
BOOL
1 = Ready for OCmd_JogRev, enable HMI button.
ORdy_Lock
BOOL
1 = Ready for OCmd_Lock, enable HMI button.
ORdy_Normal
BOOL
1 = Ready for OCmd_Normal, enable HMI button.
ORdy_Oper
BOOL
1 = Ready for OCmd_Oper, enable HMI button.
ORdy_OutDatalink
BOOL
1 = Ready for OSet_OutDatalink, enable data entry field.
ORdy_Prog
BOOL
1 = Ready for OCmd_Prog, enable HMI button.
ORdy_Reset
BOOL
1 = A latched alarm or shed condition is ready to be reset.
ORdy_ResetAckAll
BOOL
1 = A latched alarm or shed condition is ready to be reset or acknowledged.
ORdy_SpeedRef
BOOL
1 = Ready for OSet_SpeedRef, enable data entry field.
ORdy_StartFwd
BOOL
1 = Ready for OCmd_StartFwd, enable HMI button.
ORdy_StartRev
BOOL
1 = Ready for OCmd_StartRev, enable HMI button.
ORdy_Stop
BOOL
1 = Ready for OCmd_Stop, enable HMI button.
ORdy_Unlock
BOOL
1 = Ready for OCmd_Unlock, enable HMI button.
Sts_FaultDesc
STRING
Description of motor controller fault, lookup from last fault code.
Public InOut Members
Data Type
FBD Default Visibility
FBD Wiring required
Usage
Description
Ref_Ctrl_Set
RAC_ITF_DVC_PWRVELOCITY_SET
Visible
Required
InOut
Velocity Automation Device Object Settings Interface.
Ref_Ctrl_Cmd
RAC_ITF_DVC_PWRVELOCITY_CMD
Visible
Required
InOut
Velocity Automation Device Object Command Interface.
Ref_Ctrl_Sts
RAC_ITF_DVC_PWRVELOCITY_STS
Visible
Required
InOut
Velocity Automation Device Object Status Interface.
BusObj
BUS_OBJ
Visible
Required
InOut
Bus component.
Ref_FaultCodeList
RAC_CODE_DESCRIPTION[1]
Visible
Required
InOut
Fault Code to Fault Description lookup table for intelligent motor controller.
RAC_ITF_DVC_PWRVELOCITY_SET Structure
The RAC_ITF_DVC_PWRVELOCITY_SET structure is the first of three structures exchanged with the associated Power Velocity Device Object to interface with the variable speed drive device. This structure handles settings, such as the speed reference, sent to the drive.
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, other pins on the instruction are used to link the necessary data.
Members
Data Type
Description
InhibitCmd
BOOL
1 = Inhibit user Commands from external sources, 0 = Allow Commands.
InhibitSet
BOOL
1 = Inhibit user Settings from external sources, 0 = Allow Settings.
Speed
REAL
Speed reference (Hz). Valid = 0.0 to maximum drive frequency.
RAC_ITF_DVC_PWRVELOCITY_CMD Structure
The RAC_ITF_DVC_PWRVELOCITY_CMD structure is the second of three structures exchanged with the associated Power Velocity Device Object to interface with the variable speed drive device. This structure handles commands, such as start, stop and jog, sent to the drive. It is an InOut parameter configured as optional (May Be Null).
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, other pins on the instruction are used to link the necessary data.
Members
Data Type
Description
bCmd
INT
Commands (Bit Overlay):
Physical
BOOL
Operate as a physical device.
Virtual
BOOL
Operate as a virtual device.
ResetWarn
BOOL
Reset warning status.
ResetFault
BOOL
Reset fault status.
Activate
BOOL
Activate output power structure.
Deactivate
BOOL
Deactivate output power structure.
CmdDir
BOOL
Select direction: 0 = Forward, 1 = Reverse.
RAC_ITF_DVC_PWRVELOCITY_STS Structure
The RAC_ITF_DVC_PWRVELOCITY_STS structure is the third of three structures exchanged with the associated Power Velocity Device Object to interface with the variable speed drive device. This structure handles status, such as the speed feedback, active status, commanded and actual direction, received from the drive. It is an InOut parameter configured as optional (May Be Null).
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, other pins on the instruction are used to link the necessary data.
Members
Data Type
Description
eState
DINT
Enumerated state of the device object:
0 = Unused,
1 = Initializing,
2 = Disconnected,
3 = Disconnecting,
4 = Connecting,
5 = Idle,
6 = Configuring,
7 = Available.
FirstWarning
RAC_ITF_EVENT
First warning.
FirstFault
RAC_ITF_EVENT
First fault.
eCmdFail
DINT
Enumerated command failure code.
Speed
REAL
Actual Speed (Hz).
bSts
INT
Status (Bit Overlay):
Physical
BOOL
1 = Operating as a physical device.
Virtual
BOOL
1 = Operating as a virtual device.
Connected
BOOL
1 = Connected and communicating.
Available
BOOL
1 = Device is configured and can be operated.
Warning
BOOL
1 = Device has a warning.
Faulted
BOOL
1 = Device is faulted.
Ready
BOOL
1 = Device is ready to be activated.
Active
BOOL
1 = Device is active (power structure active, drive running).
ZeroSpeed
BOOL
1 = Motor is at zero speed (not rotating).
ObjCtrl
BOOL
0 = Object has control of this device, 1 = Object does not have control of this device (for example, local HIM or I/O has control).
CmdDir
BOOL
Commanded direction: 1 = Reverse, 0 = Forward
ActDir
BOOL
Actual (rotation) direction: 1 = Reverse, 0 = Forward
Accelerating
BOOL
1 = Motor is accelerating.
Decelerating
BOOL
1 = Motor is decelerating.
AtSpeed
BOOL
1 = Motor actual speed has reached speed reference.
BUS_OBJ Structure
The BUS_OBJ structure links the variable speed drive to other devices and instructions in a complex control strategy, typically into a hierarchy. A Bus Object rolls up status and alarm information from lower level devices to higher level control and fans out commands from higher level control to lower level devices, and items link to the bus by referencing a single member of the BUS_OBJ array associated with the bus.
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, the Bus functions of this instruction are not available.
Members
Data Type
Description
Inp_Cmd
DINT
Input to assert commands
Out_Cmd
DINT
Resultant commands
Inp_CmdLLH
DINT
Input for level normally high commands
Out_CmdLLH
DINT
Resultant line level high commands
Inp_Sts
DINT
Input to assert status
Out_Sts
DINT
Resultant status
Inp_CmdAck
DINT
Input to assert a command acknowledgement
Out_CmdAck
DINT
Resultant command acknowledgements
Inp_SeverityMax
DINT
Input: maximum alarm severity
Out_SeverityMax
DINT
Resultant of maximum alarm severity
Cfg_CmdMask
DINT
Propagation mask for commands
Cfg_CmdLLHMask
DINT
Propagation mask for line level high commands
Cfg_StsMask
DINT
Propagation mask for status
Ref_Index
DINT
Bus array index
RAC_CODE_DESCRIPTION[x] Structure
The RAC_CODE_DESCRIPTION[x] structure is an array of drive fault code number and fault code description pairs, used as a lookup table. The instruction searches the table for the fault code received from the drive and displays the corresponding fault description text.
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, the fault code lookup function is not performed. Fault descriptions will only be shown if provided through the Device Object Status interface.
Members
Data Type
Description
Code
DINT
Code for which to look up Description.
Desc
STRING
Description for given Code.
RAC_EVENTStructure
RAC_EVENTstructures are used by the FirstFault and FirstWarning members in the RAC_ITF_DVC_PWRVELOCITY_STS structure. These items hold the event data received from the drive for the first drive fault and first drive warning records in the drive event history.
Members
Data Type
Description
Type
DINT
Event type:
1 = Status,
2 = Warning,
3 = Fault,
4 ...n = User.
ID
DINT
User-definable event ID.
Category
DINT
User-definable category (Electrical, Mechanical, Materials, Utility, etc.).
Action
DINT
User-definable event action code.
Value
DINT
User-definable event value or fault code.
Message
STRING
Event message text.
EventTime_L
LINT
Event timestamp (64-bit microseconds format).
EventTime_D
DINT[7]
Event timestamp (year, month, day, hour, minute, second, microsecond format).
Alarms
Discrete Logix tag-based alarms are defined for these members:
Member
Alarm Name
Description
Sts_FailToStart
Alm_FailToStart
Drive failed to start within the allotted time when commanded to start.
Sts_FailToStop
Alm_FailToStop
Drive failed to stop within the allotted time when commanded to stop.
Sts_IntlkTrip
Alm_IntlkTrip
Drive stopped by an Interlock Not OK.
Sts_IOFault
Alm_IOFault
Drive communication with controller failed.
Sts_DriveFault
Alm_DriveFault
The variable speed drive is reporting it has a fault condition.
Mark the alarm as used or unused and set standard configuration members of the discrete Logix Tag based alarm. Use this format to access alarm elements:
Tag.@Alarms.AlarmName.AlarmElement
The PVSD instruction uses these alarms:
  • Raises the Fail to Start alarm when the drive is commanded to start but run feedback is not received within the configured failure time.
  • Raises the Fail to Stop alarm when the drive is commanded to stop but run feedback does not drop within the configured failure time.
  • Raises the Interlock Trip alarm when the motor is running and an interlock not-OK condition causes the motor to stop. If interlocks are not bypassed, a bypassable interlock or a non-bypassable interlock not-OK condition initiates an interlock trip. If interlocks are bypassed, only a non-bypassable interlock not-OK condition initiates an interlock trip.
  • Raises the I/O Fault alarm when I/O communication with the variable speed drive is lost. For the Power Velocity Device interface, this is detected when the Ref_Ctrl_Sts.Connected bit goes false (to 0). For the discrete signal interface, used when Ref_Ctrl_Sts is NULL, this is detected when Inp_IOFault goes true (to 1).
  • Raises the Drive Fault alarm when the drive reports a drive faulted condition. For the Power Velocity Device interface, this is detected when the Ref_Ctrl_Sts.Faulted bit goes true (to 1). For the discrete signal interface, which is used when Ref_Ctrl_Sts is NULL, this is detected when Inp_Faulted goes true (to 1).
Program, Operator, and External commands reset latched alarms, and reset and acknowledge all alarms of the instruction (Alarm Set) at the same time. This diagram shows how the commands interact with the PVSD instruction.
PVSD_alarm_operation
Operation
This diagram illustrates functionality of the PVSD instruction:
PVSD_operation_v34
The second diagram illustrates the handling of the drive speed reference (setpoint) and drive speed feedback:
PVSD_operation2
The third diagram illustrates the handling of the optional input datalink and output datalink functions:
PVSD_operation3
Monitor the PVSD Instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
Any commands received before first scan are discarded. The motor is de-energized and treated as if it were commanded to stop.
Instruction first run
Any commands received before first scan are discarded. The motor state is evaluated and the instruction aligns with the current state of the motor, as if the Hand command source were selected.
Rung-condition-in is false
Handled the same as if the motor is taken Out of Service by command. The motor outputs are de-energized, and the motor Command Source is shown as Program Out of Service on the HMI. All alarms are cleared. The rung-condition-out continues as false.
Rung-condition-in is true
Set rung-condition-out to rung-condition-in.
The instruction executes.
Postscan
Rung-condition-out is cleared to false.
Function Block Diagram
Condition/State
Action Taken
Prescan
Any commands received before first scan are discarded. The motor is de-energized and treated as if it were commanded to stop.
Instruction first run
Any commands received before first scan are discarded. The motor state is evaluated and the instruction aligns with the current state of the motor, as if the Hand command source were selected.
Instruction first scan
See instruction first run in the function block diagram table.
EnableIn is false
Handled the same as if the motor is taken Out of Service by command. The motor outputs are de-energized, and the motor Command Source is shown as Program Out of Service on the HMI. All alarms are cleared. EnableOut is set to false.
EnableIn is true
EnableOut is set to true.
The instruction executes.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic it will execute.
Condition/State
Action Taken
Prescan
See Prescan in the Function Block Diagram table.
Instruction first run
See Instruction first run in the Function Block Diagram table.
EnableIn is true
See EnableIn is true in the Function Block Diagram table.
Postscan
See Postscan in the Function Block Diagram table.
Example
In the following example, the first three reference (InOut parameter) tags are used to interface to a Power Velocity Device object, provided by Commercial Engineering. These tags provide the Speed Reference setting to the drive, the various activate (start), deactivate (stop), and clear fault commands to the drive, and drive status from the drive, including status such as active (running), actual speed, commanded and actual direction, and fault and warning information and test. The next InOut parameter links this drive to a bus of related devices, control modules, equipment modules and unit(s) in a hierarchy used to fan out commands and roll up status and alarm information for use in complex control strategies and sequences.
In this example, the Fault Code List parameter is not used because the textual fault information is received from the Power Velocity Device object, and no lookup from a fault code is required in this instance.
Ladder Diagram
PVSD_example_ladder
Function Block Diagram
PVSD_example_FBD
Structured Text
PVSD(MyNG_PVSD, MyNG_PVSD_Ctrl_Set, MyNG_PVSD_Ctrl_Cmd, MyNG_PVSD_Ctrl_Sts, MyNG_Bus[19], 0)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal