Add a group

Groups determine the organization of a system. For example, a system may have filling and packaging groups.
  1. In the main toolbar, select
    Open dashboard page
    and then select
    Manage users and groups
    .
  2. On the dashboard page, under
    Groups
    , select
    Add
    .
  3. In
    Add Group
    , under
    Name
    , enter the name for the group.
  4. (optional) If users are created, under
    Assign user to groups
    , select the users to assign to the group.
  5. (optional) If roles are created, under
    Assign roles to group
    , select the roles to assign to the group.
  6. Select
    Add
    .
    TIP: To create a group in
    Project view
    , under
    Security
    , right-click
    Groups
    to add a group, or select a group to add a subgroup, and then select
    New
    Group
    .
The new group appears on the dashboard page and in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal