Duplicate a recipe schema

Duplicate an existing recipe schema to base the new schema on the old schema.
  1. From the toolbar, select
    Open dashboard page
    .
  2. In the editor, select
    Configure a recipe
    .
  3. Right-click the available recipe schema and select
    Duplicate
    .
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal