Eclipse Mosquitto broker

Push Agent supports the following modes of communication with the Mosquitto broker.
Anonymous
Send and receive messages without authenticating with the broker.
Authenticated
Send and receive messages once authenticated with username and password.
Secured
Send and receive encrypted messages through SSL.
TIP:
Adapt the broker configuration to your needs. Select the communication mode and port.
Port 1883
Used for an anonymous/authenticated communication.
Port 8883
Used for secured communication.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal