Profile objects for different presentation engines

Create dynamic links between Boolean properties of objects and the
{Session}/IsNative
and
{Session}/IsWeb
aliases. You can then display different objects using different presentation engines.
TIP:
Download a sample project:
ProfileObjects.zip
Native presentation engine and Web presentation engine
This example shows an application that displays two different objects based on the presentation engine.
Prerequisites
  1. To profile objects for different presentation engines
  2. In
    Project view
    , select an object to profile.
    For example, select a rectangle.
  3. In
    Properties
    , create a dynamic link between a Boolean property and either:
    • Aliases
      {Session}
      Session
      UI Session
      Native session
    • Aliases
      {Session}
      Session
      UI Session
      Web session
    For more information about dynamic links, see Create dynamic links.
    For example, create a dynamic link between the
    Visible
    property of the object and
    Aliases
    {Session}
    Session
    UI Session
    Native session
    to make the object visible in the native presentation engine only.
  4. In
    Project view
    , select an object to profile.
    For example, select another rectangle.
  5. In
    Properties
    , create a dynamic link between a Boolean property and either:
    • Aliases
      {Session}
      Session
      UI Session
      Native session
    • Aliases
      {Session}
      Session
      UI Session
      Web session
    For more information about dynamic links, see Create dynamic links.
    For example, create a dynamic link between the
    Visible
    property of the object and
    Aliases
    {Session}
    Session
    UI Session
    Web session
      to make the object visible in the native presentation engine only.
The native presentation engine and web presentation engine display different objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal