Button

Generates events to perform methods.

Events

Use these button events to trigger methods:
Event
Generated at runtime when
MouseClick event
An object is clicked or touched and then released.
MouseDown event
An object is clicked or touched.
MouseUp event
The click or touch of the object is released.

Use case

Trigger different actions, for example:
  • Start report generation
  • Acknowledge active alarm
  • Signal an emergency condition

Example

Three buttons with different styles
graphic showing three different button styles
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal