OMRON Fins Driver

Observe these guidelines when working with the OMRON Fins Driver.

Supported controllers

The driver supports OMRON® CJ and CP controller families.
IMPORTANT: The driver has been tested with CJ2 controllers family.

Controller tags import

You can only import tags from TXT files in the offline mode.
IMPORTANT:
Before you import tags into
FactoryTalk Optix Studio
, from CX-Programmer, copy the symbol table into a TXT file.
For more information, refer to the product documentation.

Data types

Supported data types
Controller data type
FactoryTalk Optix
data type
Length
BOOL
BOOL
1 BIT
CHANNEL
INT16
2 BYTES
COUNTER
INT16
2 BYTES
WORD
UINT16
2 BYTES
DWORD
UINT32
4 BYTES
LWORD
UINT64
8 BYTES
INT
INT16
2 BYTES
DINT
INT32
2 BYTES
UINT
UINT16
2 BYTES
UINT_BCD
UINT16
2 BYTES
UDINT
UINT32
4 BYTES
UDINT_BCD
UINT32
4 BYTES
LINT
INT64
4 BYTES
ULINT
UINT64
8 BYTES
ULINT_BCD
UINT64
8 BYTES
REAL
FLOAT
4 BYTES
LREAL
DOUBLE
8 BYTES
TIMER
INT16
2 BYTES
STRING
STRING
LENGTH
ARRAY 1 dimensional
Type [dimension]
Supported data areas
Controller memory area
FactoryTalk Optix
memory area
Notes
CIO
CIO area
A
Auxiliary area
T
Timer
C
Counter
D
Data Memory
H
Holding area
W
Work area
Ex
EM area CurrentBank
Addresses memory location x in the current bank.
Ex_y
EM area
Addresses memory location y in bank x.
IR
Not supported
DR
Not supported
TK
Not supported
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal