CODESYS Driver

Observe these guidelines when working with CODESYS driver.

Controller tags import

You can import tags in these modes:
Online mode
Use online mode to import tags directly from the controller at design time or runtime.
Offline mode
For more information, refer to the product documentation.
This communication driver supports importing custom data types defined in the controller project in the offline mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal