Translate an alarm message

The message displayed in an
Alarms
widget is a text string that can appear in different languages. Enter a message, select the language for the translation, and then enter the translated string. The translated alarm message appears in the language of the user at runtime.
Prerequisites
  1. To translate an alarm message
  2. In
    Project view
    , navigate to and select the alarm.
  3. In
    Properties
    , in
    Message
    , type the message the alarm event is to display at runtime.
  4. In
    Project view
    , expand
    Translations
    .
  5. Double-click
    LocalizationDictionary#
  6. In the Translation Editor, select
    View
    Translation Reference
    .
    Your new message appears in the
    String
    column.
  7. In the row of the alarm message, select 
    Synchronize
    .
    A corresponding translated message appears in the
    Key
    column.
  8. Select
    View Translation Table
    .
  9. Select
    Add locale
    , select the desired language for the translation, and then select
    Checkmark
    .
  10. In
    New locales added
    , select
    Yes
    .
  11. In the third column, enter the string for the translation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal