Create Alarm manager and Alarm summary
Create an
alarm manager
and alarm summary
widgets, to display essential information about alarms in the project.- In the main toolbar, selectTemplate Libraries.Template Libraries
- InTemplate Libraries, selectWidgets.
- UnderComponents, dragAlarm WidgetstoUIfolder inProject view.AlarmSummary# (type)andAlarmManager# (type)appear in the folder.
- InTemplate Libraries, selectClose.TIP: To display the widgets at runtime, you can create a dynamic link from navigation panels. See Dynamic links.
- (optional) Configure the properties of the two widgets.You can adjust the widgets dimensions, button behavior, available alarms, and property value presets. See Configure Alarm widgets.
Provide Feedback