View alarms in UTC time zone

Alias the
Time
property of the
Alarm grid
object to view events in the UTC (Coordinated Universal Time) time zone standard. UTC is the time standard on which all time zones are based worldwide. Viewing alarms in the UTC time zone ensures that all users are seeing the same time stamps for the alarms.
  1. In the main toolbar, select
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Widgets
    .
  3. Drag the
    Alarms Grid
    object to the desired folder in the
    UI
    folder.
    AlarmGrid# (type)
    appears.
  4. In
    Template Libraries
    , select
    Close
    .
  5. In the editor, select the alarm grid and then in
    Properties
    :
    1. Expand
      Timestamp
      .
    2. Expand the
      Data grid
      category.
    3. Expand the
      Column
      category and then select
      DataItemTemplate
      .
    4. In
      Text
      , select
      Add Dynamic Link
      .
    5. In the
      Dynamic Links
      window, expand
      Aliases
      .
    6. Expand
      Alarm Condition
      and then select
      Time
      .
    7. Choose
      Select
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal