Trial Entitlements

Rockwell sales representatives can send trial entitlements to provide a trial use of applications in FactoryTalk Hub. These trials have a set length of time for use and should be allocated to be used soon after receiving them.
When you are sent a trial entitlement, you receive an email with a link that lets you sign in to FactoryTalk Hub to view and begin your trial.
NOTE: Trial Entitlements can only be viewed and allocated by administrators and owners of organizations. Contributors in an organization can see entitlements and trials that are assigned to them but cannot see the entitlements and trials allocated to the organization and cannot allocate the entitlements and trials they are assigned.
Free Trial Entitlement Screen
Select
Redeem now
to start your trial. The trial entitlement is then available in the trials tab of the View Entitlements screen. Note the expiration date and make sure to allocate and use your trial before it expires.
Trial Entitlement in the trials tab
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal