Cascading Loops (PID)
The PID cascades two loops by assigning the output in percent of the master loop to the setpoint of the slave loop. The slave loop automatically converts the output of the master loop into the correct engineering units for the setpoint of the slave loop, based on the slave loop’s values for .MAXS and .MINS.
Relay Ladder

Provide Feedback