Bitwise Not (NOT)

The NOT instruction performs a bitwise inversion of the Source and places the result in Dest.
When enabled, the instruction evaluates the bitwise NOT operation:
Dest = NOT Source
If the bit in the Source is:
The bit in the Dest is:
0
1
1
0
Available Languages
Ladder Diagram
Ladder Diagram_Bitwise Not (NOT))_v1
FactoryTalk Design Studio
DSL - Ladder Diagram
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten
  • Members of a structure operand are overwritten
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions
.
Ladder Diagram
Operand
Data Type
Format
Description
Source
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
immediate
tag
Value to NOT
//FLOAT includes REAL and LREAL data types.
Tip:
Floating point inputs are converted to integer which may cause an overflow.
Dest
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
tag
Tag to store result of the instruction.
Tip:
If the destination type is FLOAT, the resultant value will be converted to floating point.
TIP: When integer promotion is required for the inputs, the smaller type is converted to the larger type using zero extension.
Affects Math Status Flags
Conditional. See Math status flags.
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in
Dest is set as described in the Description section.
Postscan
N/A
Examples
Ladder Diagram
FTStudio-NOT-LD-EX-V1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal