One Shot (ONS)

The ONS instruction makes the remainder of the rung true each time rung-condition-in transitions from false to true.
Available Languages
Ladder Diagram
Ladder Diagram_One Shot (ONS)_v1
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten
  • Members of a structure operand are overwritten
  • Except when specified, structure operands are shared by multiple instructions.
Ladder Diagram
Operand
Data Type
Format
Description
Storage bit
BOOL
tag
Internal storage bit.
Retains the rung-condition-in from the last time the instruction was executed.
There are various operand addressing modes possible for the storage bit, see Bit Addressing for examples.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The storage bit is set to true to prevent an invalid trigger during the first scan.
Rung-condition-in is false
The storage bit is cleared to false, rung-condition-out is cleared to false.
Rung-condition-in is true
See ONS Flow Chart (True).
Postscan
N/A
ONS Flow Chart (True)
onsFlowChart
Example
Ladder Diagram
FTStudio-ONS-LD-EX-V1
In this example, the sum increments each time limit_switch_1 goes from false to true.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal