Create a trend

Create a trend to graphically plot sampled data onto a chart for up to eight tags.
To create a trend:
  1. Enter a name for the trend.
  2. Enter a description for the trend.
  3. If you wish to use a sample period that differs from the default sample period, enter a new sample period value.
  4. Select
    OK
    .
    The trend is displayed in the
    Trends
    folder in the
    Controller Organizer
    tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal