Change report preferences

The
Print Options
dialog allows you to set up the way you want your reports to appear. Simply select or clear the respective options under the various categories on the
Print Options
dialog based on the information you want to include in your reports.
For more specific information on setting up your reports, refer to the following:
The following listings also have configurable font and color options:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal