Monitor program and task properties

Use the
Properties
pane to monitor the properties of existing programs and tasks.
  1. On the explorer bar, select Execution icon
    Execution
    .
  2. Expand the controller folder.
  3. Expand the program folder to select a program or the
    Tasks
    folder to select a task.
  4. In
    Properties
    on the
    Monitor
    tab, monitor the program or task properties. For programs, the properties are shown in microseconds. For tasks, the properties are shown in milliseconds. Monitor:
    • For programs, the
      Max
      and
      Last
      Scan times
      in execution time. For tasks, the
      Max
      and
      Last
      Scan times
      in elapsed time. To clear the
      Max
      time, select
      Reset
      .
      Reset
      is available based on the project and connection state.
    • For tasks, the
      Max
      and
      Last Interval times
      in elapsed time between triggers.
    • For tasks, the
      Task overlap count
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal